Post Go back to editing

Evaluation of multiple transceivers

Category: Hardware
Product Number: ADRV9003

Hi, 

So, if I have 4 antennas, for development and evaluation purposes do I need to buy two evaluation boards ADRV9002NP/W2/PCBZ ?

Or, is there a board with 2 transceiver IC?

Are there any other method to achieve this?



Added a few more questions
[edited by: rahulpillai at 4:02 AM (GMT -5) on 6 Mar 2024]

Thread Notes

Parents
  • Hi rahulpillai,

    In some cases, for example, if your 4 antennas configuration is 2 receiver and 2 transmit (TDD or FDD), or 4 receiver (TDD with Rx port switching), you may be able to do this one on board.

    There is currently no eval board with two ADRV9002 transceivers. If you'd like to evaluate more than 2 transceiver channels, you'll need more than one board.

    Kind Regards,
    Michał

  • Hey, thanks for replying.

    My application is simplex there is no transmission, all the 4 antenna elements acts as receivers.

    What I am expecting is to receive signals from the 4 antenna elements and send it to FPGA for processing.

    If i need two evaluation boards, and all 4 receivers in the two boards are set to 2-lane LSSI with lane data rate of 983MHz per receiver channel, so, the bandwidth of one board will be around 2 * 983Mhz = 1.9Gbps. The ZC706 evaluation board, in the website it is mentioned the FMC LPC port is capable of 1GT, is it 1 giga transfer as in 1Gbps or something else?. If the LPC FMC is only capable of 1Gbps and there is only 1 FMC HPC with 8GT how can i connect two boards?

    PS: I am a beginner in working with advanced ICs, a detailed response with resource will be helpful

    Thank you.

Reply
  • Hey, thanks for replying.

    My application is simplex there is no transmission, all the 4 antenna elements acts as receivers.

    What I am expecting is to receive signals from the 4 antenna elements and send it to FPGA for processing.

    If i need two evaluation boards, and all 4 receivers in the two boards are set to 2-lane LSSI with lane data rate of 983MHz per receiver channel, so, the bandwidth of one board will be around 2 * 983Mhz = 1.9Gbps. The ZC706 evaluation board, in the website it is mentioned the FMC LPC port is capable of 1GT, is it 1 giga transfer as in 1Gbps or something else?. If the LPC FMC is only capable of 1Gbps and there is only 1 FMC HPC with 8GT how can i connect two boards?

    PS: I am a beginner in working with advanced ICs, a detailed response with resource will be helpful

    Thank you.

Children