Post Go back to editing

Temperature beyond +85 degrees

Thread Summary

The user inquired about the safe operating temperature range for the ADRV9002, specifically if it can operate above +85°C. The support engineer confirmed that the chip is designed to operate up to +110°C, and the internal temperature sensor can be used as a reference. The user followed up, asking if operating near +110°C could affect functionality and lifespan, but this concern was not addressed in the final answer.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADRV9002

Hi,

According to the datasheet, the junction temperature of the ADRV9002 is +110 degrees. So, is it safe to operate above +85 degrees? Can we use internal temperature sensor as a reference?

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.