Post Go back to editing

About the ADCs present in the ADRV9002

Thread Summary

The user inquires about the ADC configurations in the ADRV9002, specifically the number, resolution, and clock frequency of the HP and LP ADCs. The final answer confirms the presence of two 5-bit HP sigma-delta ADCs and two 16-bit LP ADCs per receiver channel, and explains that the auxiliary ADCs are 10-bit and used for real-time IC monitoring, not I/Q conversion. The user is directed to the ADRV9002 datasheet and additional Analog Devices resources for more detailed information on ADC specifications and sigma-delta ADCs.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADRV9002

Hi,

I want to use the ADRV9002 for wideband applications. While going through the data sheet I am a bit confused on the Number of ADC that are present in ADRV9002 and their resolution and clock frequency. 

From what i understand, the ADRV9002 have two HP sigma delta ADC 5-bits wide and two LP 16-bit resolution ADC for each receiver channel, along with four auxiliary ADCs each 10-bit resolution in total.

so, the auxiliary data converters is not for I/Q analog to digital conversion? and is used to send real time IC info like temperature and other measurement to baseband processor and vice versa? like what is their purpose?

This is what i could understand from the ADRV9001 manual

Where can i find information like the resolution and clock frequency of the HP sigma-delta and LP ADC in the ADRV9002 datasheet?.

Where can i find this information in the datasheet?.

  • Hi Rahul 

    ADRV9002 module consists of pair of highly linear performance ADCs and a pair of low-power ADCs as , illustrated in the Rx signal chain block diagram (Fig 1) below are used for capturing IQ signals.

                                                                      

                                                                                                    Fig 1: Rx signal chain block diagram

    The ADRV9001 supports three standard ADC clocks: ADC-H clock at 2211.84 MHz, ADC-M clock at 1474.56 MHz, and ADC-L clock at 1105.92 MHz, applicable to both high-performance (HP) and low-power (LP) ADCs (referenced in the user development guide page 141 of 351) also highlighted in the decimation stages block diagram (Fig 2). These sample rate are unrelated to the samples rate that the user provide at the data port interface which is maximum of 61.44MHz (highlighted in the decimation stages block diagram in blue color). One to be note that if arbitrary sample rate is chosen for data port sample rate then ADC/DAC sample rate will change slightly in accordance with the data port sample rate.

                                                                           

                                                                                             Fig 2: Decimation Stages Block Diagram

    ADRV9002 incorporates various built-in auxiliary functions to enhance monitoring and control capabilities. These functions comprise auxiliary ADC (4x10 bits AuxADC), auxiliary DAC (4x12 bits AuxDAC). These components are integrated to streamline control tasks, such as static voltage measurements and temperature sensing. The clock rate for the AuxADC is 30.72 MSPS (as referenced in the user development guide page 243 of 351). It's important to note that these AuxADCs are not utilized for RF IQ signals. One of the use case of using AuxADC and Aux DAC is to have a power amplifier RAMP control (as referenced in the user development guide page 233 of 351).

    More information on data converter resolution

    • In case of AuxADC the ADCs are 10 bits meaning the number of steps will be 1024 (210), since the reference voltage is 0.95V, so each bit will correspond to (1.8/(210)) = approx. 927.7 µV.

    Overall the performance of ADRV9002 is highly dependent on the use cases and specification of the ADCs, my colleague has authored an article detailing how to compute valuable performance metrics using the specifications. You can access the article here:

    https://www.analog.com/en/resources/technical-articles/high-dynamic-range-rf-transceiver-solves-the-blocking-challenge.html

    Regards,

    Mushini

  • Hello Mushini,

    Thank you for replying. 

    Could you point out the details of HP and LPADC in the ADRV9002 datasheet(not the user guide)?

    I couldn't find the page where it talks about the receiver ADC clocks and its resolution. At first I got confused with AuxADC as the receiver ADC, then later down the line when I read about the data interface in the datasheet, there they have mentioned 16-bits I/Q signals, I thought the resolution is 10-bits and the other 6-bits maybe zero padding. Reading the user guide solved the confusion for me.

    But I would really appreciate it if you could point where I can read the details of the receiver ADC(HP&LPADC) in the datasheet.

    Also if at all possible, could you provide the details on the working of 5-bit sigma-delta adc, like an article?

    Sincerely,

    rahulpillai

  • Hi Rahul,

    Thank you for reaching out.

    Our data sheets are designed to provide relevant specifications tailored to your needs. While we strive to include as much information as possible, it's important to note that datasheet provides only relevant information, as if it may not be an appropriate place for all this information. For more comprehensive insights and guidance, we recommend referring to our user development guides. These guides offer further information and assistance to ensure your needs are met effectively. Should you have any specific inquiries or require additional support, please don't hesitate to let us know. We're here to help.  Below, you'll find links to articles and an interactive tutorial that delve into the workings of delta sigma ADCs for better understanding.    

    Articles for Delta Sigma ADCs

    https://www.analog.com/media/en/technical-documentation/application-notes/292524291525717245054923680458171an283.pdf

    https://www.analog.com/media/en/technical-documentation/application-notes/28715432842357460935458165408691an388.pdf

    www.analog.com/.../behind-the-sigma-delta-adc-topology.html

    Delta Sigma ADCs Interactive tutorial

    www.analog.com/.../sigma-delta-adc-tutorial.html

    Regards,

    Mushini

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.