KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hello!
We are using TDD profile with RX1 and RX2 generated through TES and linux driver (not the API). RX enable is configured to be via SPI.
I noticed that mode stays in "PRIMED" until I manually switch it to RF_ENABLED using iio_attr binary from libiio.
Is this expected way of activating RX or should driver move RX mode to RF_ENABLED state automatically? I thought driver should take care of this but it never happens.
Am I missing some configuration or is this the way is should behave?
Thank you!
__CommunityServer__Service__ - Moved from TES GUI & Software Support ADRV9001 – ADRV9007 to Design Support ADRV9001 – ADRV9007. Post date updated from Friday, February 23, 2024 8:13 PM UTC to Thursday, January 22, 2026 10:53 PM UTC to reflect the move.
So my question is this: driver is only used for initial configuring using stream+profile but it is not responsible for setting rx to enabled in TDD? User space application should do this? (Or fpga?) Or should driver take care of this?
Once chip is configured via driver we still need app that will enable the rx?
In FDD mode, nothing is required except driver init?
Thank you in advance ;)
Hi Katarina,
User space application functions typically calls corresponding device driver functions (see software stack image on page 32 of user guide).
I assume that most of commands/functions generated in application code generated by TES are just wrapper functions with their lower-level implementations in the driver code. Some of this driver code is written/implemented on the FPGA such as automated TDD feature.
When you connect to the device in TES, and click program, the device should go to calibrated state. Then it depends, what you need to do, if you start receiving the state goes automatically to RF enabled. If you stop receiving then it goes back to primed, etc.
Regarding the difference in operation between TDD and FDD mode when using libiio, I believe the code below sheds light on this inconsistency:
The difference in operation you observed is expected. Because in TDD (where only Rx or Tx is enabled, never both simultaneously) driver cannot know if user wants to go to Rx or Tx first, so it leaves the device in Primed state. In FDD, it puts everything in RF Enabled state.
Best,
Stefan