Post Go back to editing

ADRV900x Xilinx interface IP - cutout TDD functionality / IP documentation

Thread Summary

The user inquired about configuring the ADI ADRV900x interface IP block for use with a Xilinx FPGA without TDD functionality. The final answer confirmed that TDD can be disabled within Navassa by setting the enables to active high. The engineer also provided a link to detailed AXI register documentation in PDF format, available from the ADRV9001_Regs.zip file.
AI Generated Content
Category: Hardware
Product Number: ADRV900x

We have been using the ADI ADRV900x interface IP block with a Xilinx FPGA without problem.  However, our application does not use TDD mode and I see that a large proportion of this IP block in terms of synthesised logic is devoted to TDD functionality, this logic being redundant for us.  Is there any means of configuring the core without this TDD functionality ?  Alternatively, is there any detailed documentation for this IP, including details of the AXI registers so that I may rewrite it to just include the required functionality.

Parents Reply Children
No Data