Post Go back to editing

Profile AND Frequency hopping

Product Number: ADRV9002
Software Version: 2021R2

Issue1:I want to redifine my baseband signal for my frequency hopping project.I add the config Frequencyhopping in DMA_EXAMPLE.And I use a fuction control the gpio.GPIO control is working,but I found my oscilloscope has no waveform.In my opinion,I want to modify the dma data.but now It doesn't seem to produce a waveform. . I'm not good at changing code so I used Noos DMA_EXAMPLE.I don't know how to properly boot my baseband to frequencyhopping .Have some Frequnecyhopping code to refer to?

issue2:when I genarate profile with TES, it's json  format.But the code need  string like Navassa_CMOS_profile.h.When I use it ,I need modify Navassa_CMOS_profile.h against .json file.Is there an easier way?

Issue3:When I used latest master,I noticed HDL-master named hdl-main,and I use hdl main and no-os master. When I add xsa into no-os project . and make ,CMD  print “The specified path cannot be found”.

Top Replies

  • Hi  ,

    It seems like you are running adrv900x based on no-OS example. There could be many reasons why you're not seeing output waveform.

    Could you please provide a more concrete error message? Or…