Post Go back to editing

Is there a way to measure TX/RX and RX/TX switching time on ADRV9002 under TDD mode?

Thread Summary

The user asked how to measure TX/RX and RX/TX switching time of ADRV9002 in TDD mode on the Navassa eval board. The final answer indicates that in Automated TDD mode, GPIO pins can be assigned to Rx1 and Tx1 to reflect the Rx/Tx enable signals, and the switching time can be measured using a logic analyzer. The TDD Enablement Delays tab in TES provides more accurate details on switching time.
AI Generated Content
Category: Hardware
Product Number: ADRV9002

How can we measure the TX/RX and RX/TX switching time of ADRV9002 under TDD mode? Is there access on the Navassa eval board?

Thread Notes

Parents Reply
  • In automated TDD assigning GPIO to Rx1 or Tx1 pins means that those eval board GPIO pins will reflect the Rx/Tx enable signals, as shown in the timing diagram in TES (once you enable automated TDD checkbox).

    If you want to enable Tx/Rx through GPIOs then you would need to choose "Pin" as channel enablement mode in TES->Radio->Radio Control. Please also see TDD Enablement Delays tab in TES to find more accurate details on switching time.  

Children
No Data