How can we measure the TX/RX and RX/TX switching time of ADRV9002 under TDD mode? Is there access on the Navassa eval board?
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
How can we measure the TX/RX and RX/TX switching time of ADRV9002 under TDD mode? Is there access on the Navassa eval board?
Dorant - Moved from RF and Microwave to Design Support ADRV9001 – ADRV9007. Post date updated from Friday, December 1, 2023 to Monday, December 4, 2023 to reflect the move.
In TES->Automated TDD tab, you should be able to enable Rx1 Pin and Tx1 Pin, assign GPIOs to them, and measure time between those pin toggles with logic analyzer.
-Stefan
What do those pins do? Do they toggle to enable TX/RX or when they are toggled the TX/RX are already up?
What do those pins do? Do they toggle to enable TX/RX or when they are toggled the TX/RX are already up?
In automated TDD assigning GPIO to Rx1 or Tx1 pins means that those eval board GPIO pins will reflect the Rx/Tx enable signals, as shown in the timing diagram in TES (once you enable automated TDD checkbox).
If you want to enable Tx/Rx through GPIOs then you would need to choose "Pin" as channel enablement mode in TES->Radio->Radio Control. Please also see TDD Enablement Delays tab in TES to find more accurate details on switching time.