Post Go back to editing

TES Configuration for ADRV9002 Custom TDD HDL Design

Thread Summary

The user is experiencing inconsistent initial calibration failures with the ADRV9002 when using modified frequency hop tables in the TES. The support engineer confirmed that the initial calibration should always work the first time and suggested that the issue might be related to the FPGA or HDL configuration. The user should verify that the ADRV9002 is under identical conditions during both successful and failed calibrations, and consider implementing a retry mechanism for the initial calibration process.
AI Generated Content
Category: Software

Hi EZ,

I am working with ADRV9002 Evaluation Board. For that, I have customized the FPGA reference design, removing all the DMA IP cores and including custom TX/RX AXI-Stream IP cores and a custom TDD HDL design that will include frequency hopping. When I say custom TDD design I mean that my custom design is generating HOP, TX_SETUP and RX_SETUP signals with specific constraints outside AXI ADRV9001 IP Core, so I have disconnected these outputs from the AXI ADRV9001 IP. These signals are generated inside my HDL IP Core. 

For the software comanding the ADRV9001 initialization, I am generating the C99 sample code from the TES.

My question is: Do I need to configure the Auto TDD tab in the TES even if I am not using the HOP, TX_SETUP and RX_SETUP signals provided by the AXI ADRV9001 IP core?

I ask this because I am facing some problems related to the RX data, the same problem that is exposed in this post:

 ADRV9002 FH-TDD solutions 

The answer for that post was that the Auto TDD state machine should be enabled, but I am not sure if that will solve my problem (at the moment is not solving it) as I am generating the FH signals externally to the AXI ADRV9001 IP core.

Thank you in advance!

Kind Regards,

Sergio.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.