Post Go back to editing

9002 dac clk from fpga 9001 side

Category: Hardware
Product Number: adrv9002

i have a 9002 setup for cmos 4 lane ddr.

so it should be doing 20 Msps. 

my question is on the 9001 side IP. 

How/where does the dac_clk get set to match the 9002?

there is an option in 9001 IP to use RX (adc clock) for tx (dac).

will that force the same clock to be used on both SSI directions and have it be controlled by 9002 config(via Spi)

Parents Reply
  • I generate the code form TES. i make the profile then have it generate the C99 code.

    My PL is using the HDL adrv9001 on a zedboard.

    i configure the 9002 via API commands. Then i configure the PL adrv9001 from my own driver using data/files generated from C99 output of TES.

    By Good Configuration meaning it is not acting like TES is telling me it should.

    TES is set to 20 Msps for Tx and Rx. Interface and Data port are the same 20 Msps in 4 Lane CMOS DDR mode. 

    In Vivado i can see with ILA that the dac_valid_i0 is not staying high. it goes high every other clock cycle.

    However, the adc_1_valid_i0 signal is high all the time. That seems correct. I would think they should act the same since they are supposed to be configured the same way.

Children
  • We can help you with the configuration of ADRV9002 via API command but the HDL is supported in the fpga forum.

    My suggestion woudl be,

    1. Verify TX and RX logics inside FPGA using loopback instead of going through ADRV9002

    2. Conifgure ADRV9002 in SSI loopback mode and see whether you are able to receive what you transmit.

    Does this make sense to you?

    -YH