Post Go back to editing

9002 register settings for DAC Channel RATE

Thread Summary

The user is configuring the DACs on the ADRV9002 and is unsure about the settings for the clock registers. The final answer clarifies that the DAC rate is not configurable and is determined by the generated profile. The user should refer to the SDK reference design documentation for correct configuration, as the Wiki documentation does not apply.
AI Generated Content
Category: Hardware
Product Number: 9002

I am using the adrv9002 and have something running but i do not think i have a good configuration for DACs.

I used TES to generate the code to give me 20Msps.

I use the API for the spi portion of configuration.

I am manually configuring the FPGA9001 portion.

I have a question on the clock registers for the DAC on the following:

0x004c REG_RATECNTRL DAC   is read write

0x0054 REG_STATUS1  read only

0x0058 REG_STATUS2 read only

I am using the info from here https://wiki.analog.com/resources/eval/user-guides/adrv9002/axi_adrv9002#dac_common_axi_ad

What am i supposed to read for registers 0x0054 REG_STATUS1 ?

I am getting 0x0.

For the clock rato 0x0058 REG_STATUS2 i am getting 4.

What would i set 0x004c REG_RATECNTRL DAC  to?

The description says "The effective dac rate (the maximum possible rate is dependent on the interface clock). The samples are generated at 1/RATE of the interface clock. "

I am running from a Zedboard with so i the clock is 100MHz.

Would i set the RateCntl to 5 so i get 100 / 5 = 20 Msps?

My TES config is for 20 Msps using DDR CMOS 4 lanes.

Thanks

Thread Notes