ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
I am using the adrv9002 and have something running but i do not think i have a good configuration for DACs.
I used TES to generate the code to give me 20Msps.
I use the API for the spi portion of configuration.
I am manually configuring the FPGA9001 portion.
I have a question on the clock registers for the DAC on the following:
0x004c REG_RATECNTRL DAC is read write
0x0054 REG_STATUS1 read only
0x0058 REG_STATUS2 read only
I am using the info from here https://wiki.analog.com/resources/eval/user-guides/adrv9002/axi_adrv9002#dac_common_axi_ad
What am i supposed to read for registers 0x0054 REG_STATUS1 ?
I am getting 0x0.
For the clock rato 0x0058 REG_STATUS2 i am getting 4.
What would i set 0x004c REG_RATECNTRL DAC to?
The description says "The effective dac rate (the maximum possible rate is dependent on the interface clock). The samples are generated at 1/RATE of the interface clock. "
I am running from a Zedboard with so i the clock is 100MHz.
Would i set the RateCntl to 5 so i get 100 / 5 = 20 Msps?
My TES config is for 20 Msps using DDR CMOS 4 lanes.
Thanks
__CommunityServer__Service__ - Moved from TES GUI & Software Support ADRV9001 – ADRV9007 to Design Support ADRV9001 – ADRV9007. Post date updated from Friday, October 20, 2023 4:31 PM UTC to Wednesday, January 28, 2026 6:52 PM UTC to reflect the move.
Moving this case to the right forum.
This is for the SDK reference design and not the GitHub based design. So any doc on the Wiki won't apply.
Moving to correct forum.
-Travis
is there an equivalent document for the SDK reference design?
Hi,
We are currently auditing our engineerzone forums for questions that have not been fully answered. If any more information is needed, please reply to this post or create a new post.
The DAC rate of the ADRV9002 is not configurable. The DAC rate will be selected based on the generated profile for the ADRV9002.
Regards,
Conrad