Post Go back to editing

About the ADRV9004 DAC and ADC bits

Thread Summary

The user inquired about the resolution of the TX DAC and RX ADC in the ADRV9004, similar to the 12-bit resolution in AD9361. The final answer provided that the ADRV9004 DAC is 16 bits, and the RX has two ADCs: a 16-bit low power ADC and a 5-bit CTDS high performance ADC. The user found this information helpful.
AI Generated Content

Hi, I'm trying to find out some information to compare the performance between AD9361 and ADRV9004. In AD9361 datasheet, it tells the resolution of both TX DAC and RX ADC are both 12 bits, but I don't find the similar parameters in ADRV9004 datasheet. Could you give me that number please?

thanks,

Jason

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.