Post Go back to editing

ADRV9002 used for measuring scattering parameters

Category: Hardware
Product Number: ADRV9002

Hi,

I am planning to use ADRV9002 for setting up an instrumentation that can measure scattering parameters. S11 and S21. For this I need three receivers (V1+, V1-, V2-) to be able to calculate S11 and S21. 

question: 1) From the datasheet I understand there are Rx1 and Rx2. However, what is the difference in Rx1A and Rx1B? is it multiplexed and simultaneously be used to to demodulate/receive the same carrier frequency? since I only have two receivers, would I need another transceiver chip?

question: 2) the power level of the Tx, does it have to be calibrated with a loopback? and after calibration would it be stable? 

question: 3) could the V1+ be obtained with the internal loop back? I understand it uses one of the receivers?

question: 4) on page 112 of UG-1828, "Transmitter NCO internal Signal Source"--> can this feature be used as the source/input signal for this type of measurement? Some more elaboration on how will be very helpful.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.