Hello,
I am wondering if there are more details on the power stage design for the ADRV9001/EVAL-ADRV9002 than already present in the ADRV9001 System Development User Guide, or some reference simulations one can obtain.
Specifically, my question is related to the feedforward capacitor from VOUTx to the FBx pin on the ADP5056, used to "improve transient performance" according to the ADP5056 Datasheet. I notice in other reference designs for the ADP5056, this capacitor is 180 pF. However, slightly more involved filters employing 10 nF capacitors and some resistors are used on the ADRV9001. Would it be possible to gain more insight as to why this was done?
Thank you in advance,
T. Stana