Post Go back to editing

ADRV9002 Loopback Rx to Tx

Thread Summary

The user inquired about setting up an internal loopback from Rx to Tx on the ADRV9002 Evaluation Board using TES. The solution involved enabling the 'Rx1 Datapath to Tx1 Datapath loopback' feature, which was confirmed to work. For a 20ms delay, the user was advised to implement the loopback at the baseband processor, as the ADRV9002's FIR filters cannot achieve such a delay. The user also asked about enabling this loopback in JupiterSDR, which is not compatible with TES, suggesting the need for a custom implementation.
AI Generated Content
Category: Hardware
Product Number: ADRV9002
Software Version: TES 0.21.0

I would like to create a loopback within the ADRV9002 Evaluation Board that takes a received signal, say an analog FM with a 1kHz tone, and loops it back out the Tx path. Is it possible to do this with TES?

Page 24 of the ADRV9002 User Guide shows what looks like a loopback path from Rx to Tx. Is that correct? Does checking the TES box next to "Enable Rx1 Datapath to Tx1 Datapath loopback in ADRV9002" in Advanced Features provide this function?

      

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.