Post Go back to editing

Regarding support in bringing up the ADRV9002 driver in the petalinux

Hiii,

This is regarding support in bringing up the ADRV9002 driver in the petalinux for the following board.
we are facing two issues in
1 : First issue during the profile upload
2 : Second one regarding the Frequency hopping enabled error .

The brief of the both points are below and also attaching the log with this query .

 1 : I was trying to upload the configuration profile file (.json) using the cat "file_name.json > profile_config" command.but after hitting the enter i got the
error "Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board." we also have checked the power and clock. 
power is okay and clock checked on the DSO that is generating.i am attaching the point 1 logs below :-

xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.bin > stream_config
xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.json > profile_config
[ 3698.162265] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
[ 3698.197278] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
[ 3698.230896] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)
[ 3699.598724] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
[ 3699.633727] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
[ 3699.667339] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)

2 : Second point regarding the frequency hopping error . I gave the  iio_info | grep iio:device command to check  the status , i got the variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.After reading the source code we found that  we can enable frequency hopping only from the profile configuration file .which we are not able to upload mentioned in point 1. We are not able to understand how to resolve both issues . Please give us the support to resolve these issues .
 2nd log below :

root@xilinx-uetc:~# iio_info | grep iio:device
iio:device0: ams
iio:device1: adrv9002-phy
[ 92.079575] adrv9002 spi1.0: Frequency hopping not enabled
[ 92.085189] adrv9002 spi1.0: Frequency hopping not enabled
9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.

[ 92.135566] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
[ 92.162670] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
[ 92.174397] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
[ 92.205153] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
[ 92.232255] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
[ 92.244006] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
[ 92.274757] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
[ 92.301855] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
[ 92.313542] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
[ 92.344287] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
[ 92.371392] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
iio:device2: axi-adrv9002-rx-lpc (buffer capable)
iio:device3: axi-adrv9002-rx2-lpc (buffer capable)
iio:device4: axi-core-tdd (label: axi-core-tdd-1)
iio:device5: axi-core-tdd (label: axi-core-tdd-2)
iio:device6: axi-adrv9002-tx-lpc (buffer capable)
iio:device7: axi-adrv9002-tx2-lpc (buffer capable)

Parents
  • Hi

    In the design, we are using single ended clock source to DEV_CLK_IN+ (40MHz) and the other pin DEV_CLK_IN- is connected to ground. Attached the schematic snapshot. Is there any way to resolve this issue ?

  • Hi,

    That ARM related error looks to be related with HW issues. Either that or, hopefully, it's just a matter of a mismatched profile. Which version of the driver are you using? Can you paste a complete boot log before trying to add any profile? Also important is, which version of TES are you using to generate the profiles?

    - Nuno Sá

  • Hii Nuno Sa,

                         Thanks for reply.

                          Driver Version :- adrv9002 spi1.0: adrv9002-phy Rev 12.0, Firmware 0.20.0.10,Stream 0.7.9.0, API version: 48.49.2 

                         TES version  :-  Navis-0.20.0.  

    i am also pasting the log here .

    U-Boot 2021.01 (Jun 01 2021 - 11:54:06 +0000)

    Board: Xilinx ZynqMP
    DRAM: 2 GiB
    PMUFW: v1.1
    EL Level: EL2
    Chip ID: zu9eg
    NAND: ERROR:arasan_nand_reset timedout
    ERROR:arasan_nand_cmd_function:command:0xff
    ERROR:arasan_nand_read_buf timedout:Buff RDY
    ERROR:arasan_nand_read_buf timedout:Xfer CMPLT
    2048 MiB
    MMC:
    Loading Environment from SPIFlash... SF: Detected mt25qu02g with page size 256 Bytes, erase size 64 KiB, total 256 MiB
    *** Warning - bad CRC, using default environment

    In: serial
    Out: serial
    Err: serial
    Bootmode: QSPI_MODE
    Reset reason: EXTERNAL
    Net:
    ZYNQ GEM: ff0d0000, mdio bus ff0d0000, phyaddr -1, interface rgmii-id
    ZYNQ GEM: requesting PHY reset gpio 70

    Warning: ethernet@ff0d0000 (eth0) using random MAC address - 12:be:0b:e5:34:15
    eth0: ethernet@ff0d0000
    Hit any key to stop autoboot: 0
    SF: Detected mt25qu02g with page size 256 Bytes, erase size 64 KiB, total 256 MiB
    device 0 offset 0x3e80000, size 0x80000
    SF: 524288 bytes @ 0x3e80000 Read: OK
    QSPI: Trying to boot script at 20000000
    ## Executing script at 20000000
    Trying to load boot images from qspi0
    SF: Detected mt25qu02g with page size 256 Bytes, erase size 64 KiB, total 256 MiB
    device 0 offset 0x3f00000, size 0x3700000
    SF: 57671680 bytes @ 0x3f00000 Read: OK
    ## Loading kernel from FIT Image at 10000000 ...
    Using 'conf-system-top.dtb' configuration
    Trying 'kernel-1' kernel subimage
    Description: Linux kernel
    Created: 2022-04-01 15:02:14 UTC
    Type: Kernel Image
    Compression: gzip compressed
    Data Start: 0x10000100
    Data Size: 11092900 Bytes = 10.6 MiB
    Architecture: AArch64
    OS: Linux
    Load Address: 0x00080000
    Entry Point: 0x00080000
    Hash algo: sha256
    Hash value: 3c5686689f1b48f7c775985ec21ab71289c87f1146c75352f513fff2204b942e
    Verifying Hash Integrity ... sha256+ OK
    ## Loading ramdisk from FIT Image at 10000000 ...
    Using 'conf-system-top.dtb' configuration
    Trying 'ramdisk-1' ramdisk subimage
    Description: petalinux-image-minimal
    Created: 2022-04-01 15:02:14 UTC
    Type: RAMDisk Image
    Compression: uncompressed
    Data Start: 0x10a9eca0
    Data Size: 45092799 Bytes = 43 MiB
    Architecture: AArch64
    OS: Linux
    Load Address: unavailable
    Entry Point: unavailable
    Hash algo: sha256
    Hash value: fb2b57e931b4740ec05786a02ee2dd20daa13d1909197f38811048baaf22c2a8
    Verifying Hash Integrity ... sha256+ OK
    ## Loading fdt from FIT Image at 10000000 ...
    Using 'conf-system-top.dtb' configuration
    Trying 'fdt-system-top.dtb' fdt subimage
    Description: Flattened Device Tree blob
    Created: 2022-04-01 15:02:14 UTC
    Type: Flat Device Tree
    Compression: uncompressed
    Data Start: 0x10a945b4
    Data Size: 42524 Bytes = 41.5 KiB
    Architecture: AArch64
    Hash algo: sha256
    Hash value: ef552f9d3b1bf312356cf183eced66087ac6af936ab2f1cc2dd99f4968426b48
    Verifying Hash Integrity ... sha256+ OK
    Booting using the fdt blob at 0x10a945b4
    Uncompressing Kernel Image
    Loading Ramdisk to 7b211000, end 7dd11fbf ... OK
    Loading Device Tree to 000000007b203000, end 000000007b21061b ... OK

    Starting kernel ...

    [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [ 0.000000] Linux version 5.10.0-xilinx-v2021.1 (oe-user@oe-host) (aarch64-xilinx-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP Fri Apr 1 15:02:14 UTC 2022
    [ 0.000000] Machine model: xlnx,zynqmp
    [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
    [ 0.000000] printk: bootconsole [cdns0] enabled
    [ 0.000000] efi: UEFI not found.
    [ 0.000000] [Firmware Bug]: Kernel image misaligned at boot, please fix your bootloader!
    [ 0.000000] cma: Reserved 256 MiB at 0x000000006b000000
    [ 0.000000] Zone ranges:
    [ 0.000000] DMA [mem 0x0000000000000000-0x000000003fffffff]
    [ 0.000000] DMA32 [mem 0x0000000040000000-0x000000007fefffff]
    [ 0.000000] Normal empty
    [ 0.000000] Movable zone start for each node
    [ 0.000000] Early memory node ranges
    [ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fefffff]
    [ 0.000000] Zeroed struct page in unavailable ranges: 256 pages
    [ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000007fefffff]
    [ 0.000000] psci: probing for conduit method from DT.
    [ 0.000000] psci: PSCIv1.1 detected in firmware.
    [ 0.000000] psci: Using standard PSCI v0.2 function IDs
    [ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [ 0.000000] psci: SMC Calling Convention v1.2
    [ 0.000000] percpu: Embedded 22 pages/cpu s50968 r8192 d30952 u90112
    [ 0.000000] Detected VIPT I-cache on CPU0
    [ 0.000000] CPU features: detected: ARM erratum 845719
    [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515844
    [ 0.000000] Kernel command line: earlycon console=ttyPS0,115200 clk_ignore_unused cpuidle.off=1
    [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [ 0.000000] software IO TLB: mapped [mem 0x000000003bfff000-0x000000003ffff000] (64MB)
    [ 0.000000] Memory: 1650688K/2096128K available (15872K kernel code, 1690K rwdata, 11976K rodata, 2624K init, 516K bss, 183296K reserved, 262144K cma-reserved)
    [ 0.000000] rcu: Hierarchical RCU implementation.
    [ 0.000000] rcu: RCU event tracing is enabled.
    [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [ 0.000000] GIC: Using split EOI/Deactivate mode
    [ 0.000000] random: get_random_bytes called from start_kernel+0x31c/0x524 with crng_init=0
    [ 0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
    [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
    [ 0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
    [ 0.008424] Console: colour dummy device 80x25
    [ 0.012481] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
    [ 0.022841] pid_max: default: 32768 minimum: 301
    [ 0.027588] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [ 0.034786] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [ 0.043605] rcu: Hierarchical SRCU implementation.
    [ 0.047524] EFI services will not be available.
    [ 0.051963] smp: Bringing up secondary CPUs ...
    [ 0.056693] Detected VIPT I-cache on CPU1
    [ 0.056733] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [ 0.057135] Detected VIPT I-cache on CPU2
    [ 0.057159] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [ 0.057539] Detected VIPT I-cache on CPU3
    [ 0.057562] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [ 0.057610] smp: Brought up 1 node, 4 CPUs
    [ 0.091780] SMP: Total of 4 processors activated.
    [ 0.096452] CPU features: detected: 32-bit EL0 Support
    [ 0.101556] CPU features: detected: CRC32 instructions
    [ 0.106694] CPU: All CPU(s) started at EL2
    [ 0.110736] alternatives: patching kernel code
    [ 0.116230] devtmpfs: initialized
    [ 0.122758] Registered cp15_barrier emulation handler
    [ 0.123451] Registered setend emulation handler
    [ 0.128054] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [ 0.137636] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [ 0.150413] pinctrl core: initialized pinctrl subsystem
    [ 0.151082] NET: Registered protocol family 16
    [ 0.155758] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [ 0.161482] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [ 0.169204] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [ 0.177033] audit: initializing netlink subsys (disabled)
    [ 0.182437] audit: type=2000 audit(0.116:1): state=initialized audit_enabled=0 res=1
    [ 0.182762] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [ 0.196854] ASID allocator initialised with 65536 entries
    [ 0.220063] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [ 0.221121] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [ 0.227794] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [ 0.234455] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [ 1.300186] DRBG: Continuing without Jitter RNG
    [ 1.377909] raid6: neonx8 gen() 2148 MB/s
    [ 1.445966] raid6: neonx8 xor() 1597 MB/s
    [ 1.514033] raid6: neonx4 gen() 2191 MB/s
    [ 1.582090] raid6: neonx4 xor() 1566 MB/s
    [ 1.650166] raid6: neonx2 gen() 2078 MB/s
    [ 1.718221] raid6: neonx2 xor() 1436 MB/s
    [ 1.786285] raid6: neonx1 gen() 1770 MB/s
    [ 1.854344] raid6: neonx1 xor() 1219 MB/s
    [ 1.922414] raid6: int64x8 gen() 1438 MB/s
    [ 1.990474] raid6: int64x8 xor() 771 MB/s
    [ 2.058544] raid6: int64x4 gen() 1602 MB/s
    [ 2.126598] raid6: int64x4 xor() 817 MB/s
    [ 2.194687] raid6: int64x2 gen() 1398 MB/s
    [ 2.262742] raid6: int64x2 xor() 748 MB/s
    [ 2.330804] raid6: int64x1 gen() 1033 MB/s
    [ 2.398882] raid6: int64x1 xor() 517 MB/s
    [ 2.398920] raid6: using algorithm neonx4 gen() 2191 MB/s
    [ 2.402878] raid6: .... xor() 1566 MB/s, rmw enabled
    [ 2.407809] raid6: using neon recovery algorithm
    [ 2.412799] iommu: Default domain type: Translated
    [ 2.417456] SCSI subsystem initialized
    [ 2.421110] usbcore: registered new interface driver usbfs
    [ 2.426433] usbcore: registered new interface driver hub
    [ 2.431710] usbcore: registered new device driver usb
    [ 2.436828] mc: Linux media interface: v0.10
    [ 2.440955] videodev: Linux video capture interface: v2.00
    [ 2.446451] EDAC MC: Ver: 3.0.0
    [ 2.449896] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels.
    [ 2.458256] jesd204: found 0 devices and 0 topologies
    [ 2.463026] FPGA manager framework
    [ 2.466491] Advanced Linux Sound Architecture Driver Initialized.
    [ 2.472806] Bluetooth: Core ver 2.22
    [ 2.475982] NET: Registered protocol family 31
    [ 2.480383] Bluetooth: HCI device and connection manager initialized
    [ 2.486700] Bluetooth: HCI socket layer initialized
    [ 2.491542] Bluetooth: L2CAP socket layer initialized
    [ 2.496566] Bluetooth: SCO socket layer initialized
    [ 2.501722] clocksource: Switched to clocksource arch_sys_counter
    [ 2.507595] VFS: Disk quotas dquot_6.6.0
    [ 2.511397] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [ 2.522295] NET: Registered protocol family 2
    [ 2.522860] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [ 2.531015] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [ 2.538960] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
    [ 2.546320] TCP: Hash tables configured (established 16384 bind 16384)
    [ 2.552678] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [ 2.559312] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [ 2.566481] NET: Registered protocol family 1
    [ 2.570997] RPC: Registered named UNIX socket transport module.
    [ 2.576581] RPC: Registered udp transport module.
    [ 2.581244] RPC: Registered tcp transport module.
    [ 2.585915] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [ 2.592903] PCI: CLS 0 bytes, default 64
    [ 2.596319] Trying to unpack rootfs image as initramfs...
    [ 4.799756] Freeing initrd memory: 44032K
    [ 4.800309] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [ 4.805436] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [ 4.813788] Initialise system trusted keyrings
    [ 4.817448] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [ 4.824453] NFS: Registering the id_resolver key type
    [ 4.828769] Key type id_resolver registered
    [ 4.832908] Key type id_legacy registered
    [ 4.836903] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [ 4.843561] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
    [ 4.886144] NET: Registered protocol family 38
    [ 4.886187] xor: measuring software checksum speed
    [ 4.893883] 8regs : 2363 MB/sec
    [ 4.897544] 32regs : 2799 MB/sec
    [ 4.902497] arm64_neon : 2380 MB/sec
    [ 4.902681] xor: using function: 32regs (2799 MB/sec)
    [ 4.907708] Key type asymmetric registered
    [ 4.911769] Asymmetric key parser 'x509' registered
    [ 4.916632] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
    [ 4.923967] io scheduler mq-deadline registered
    [ 4.928463] io scheduler kyber registered
    [ 4.959226] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [ 4.963284] cacheinfo: Unable to detect cache hierarchy for CPU 0
    [ 4.970531] brd: module loaded
    [ 4.975034] loop: module loaded
    [ 4.975309] Registered mathworks_ip class
    [ 4.978555] libphy: Fixed MDIO Bus: probed
    [ 4.981611] tun: Universal TUN/TAP device driver, 1.6
    [ 4.985713] CAN device driver interface
    [ 4.990092] usbcore: registered new interface driver asix
    [ 4.994812] usbcore: registered new interface driver ax88179_178a
    [ 5.000853] usbcore: registered new interface driver cdc_ether
    [ 5.006645] usbcore: registered new interface driver net1080
    [ 5.012266] usbcore: registered new interface driver cdc_subset
    [ 5.018148] usbcore: registered new interface driver zaurus
    [ 5.023695] usbcore: registered new interface driver cdc_ncm
    [ 5.029994] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [ 5.035776] ehci-pci: EHCI PCI platform driver
    [ 5.040548] usbcore: registered new interface driver uas
    [ 5.045500] usbcore: registered new interface driver usb-storage
    [ 5.051489] usbcore: registered new interface driver usbserial_generic
    [ 5.057935] usbserial: USB Serial support registered for generic
    [ 5.063907] usbcore: registered new interface driver ftdi_sio
    [ 5.069608] usbserial: USB Serial support registered for FTDI USB Serial Device
    [ 5.076881] usbcore: registered new interface driver upd78f0730
    [ 5.082757] usbserial: USB Serial support registered for upd78f0730
    [ 5.090319] rtc_zynqmp ffa60000.rtc: registered as rtc0
    [ 5.094181] rtc_zynqmp ffa60000.rtc: setting system clock to 2035-10-16T11:33:10 UTC (2076147190)
    [ 5.103030] i2c /dev entries driver
    [ 5.108126] usbcore: registered new interface driver uvcvideo
    [ 5.112157] USB Video Class driver (1.1.1)
    [ 5.117142] Bluetooth: HCI UART driver ver 2.3
    [ 5.120636] Bluetooth: HCI UART protocol H4 registered
    [ 5.125737] Bluetooth: HCI UART protocol BCSP registered
    [ 5.131029] Bluetooth: HCI UART protocol LL registered
    [ 5.136116] Bluetooth: HCI UART protocol ATH3K registered
    [ 5.141490] Bluetooth: HCI UART protocol Three-wire (H5) registered
    [ 5.147742] Bluetooth: HCI UART protocol Intel registered
    [ 5.153083] Bluetooth: HCI UART protocol QCA registered
    [ 5.158284] usbcore: registered new interface driver bcm203x
    [ 5.163906] usbcore: registered new interface driver bpa10x
    [ 5.169443] usbcore: registered new interface driver bfusb
    [ 5.174893] usbcore: registered new interface driver btusb
    [ 5.180352] usbcore: registered new interface driver ath3k
    [ 5.185847] EDAC MC: ECC not enabled
    [ 5.189449] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [ 5.201754] sdhci: Secure Digital Host Controller Interface driver
    [ 5.207566] sdhci: Copyright(c) Pierre Ossman
    [ 5.211888] sdhci-pltfm: SDHCI platform and OF driver helper
    [ 5.217858] ledtrig-cpu: registered to indicate activity on CPUs
    [ 5.223494] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [ 5.229926] zynqmp_firmware_probe Platform Management API v1.1
    [ 5.235680] zynqmp_firmware_probe Trustzone version v1.0
    [ 5.293548] zynqmp-aes firmware:zynqmp-firmware:zynqmp-aes: will run requests pump with realtime priority
    [ 5.313450] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
    [ 5.314185] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [ 5.319709] usbcore: registered new interface driver usbhid
    [ 5.325070] usbhid: USB HID core driver
    [ 5.335397] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found
    [ 5.337740] axi_sysid 85000000.axi-sysid-0: system ID header version mismatch. Expected 2, Reported 0
    [ 5.346765] axi_sysid: probe of 85000000.axi-sysid-0 failed with error -14
    [ 5.354025] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [ 5.360452] usbcore: registered new interface driver snd-usb-audio
    [ 5.367759] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [ 5.374268] Initializing XFRM netlink socket
    [ 5.377957] NET: Registered protocol family 10
    [ 5.382714] Segment Routing with IPv6
    [ 5.386083] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [ 5.392160] NET: Registered protocol family 17
    [ 5.396235] NET: Registered protocol family 15
    [ 5.400714] can: controller area network core
    [ 5.404984] NET: Registered protocol family 29
    [ 5.409377] can: raw protocol
    [ 5.412312] can: broadcast manager protocol
    [ 5.416466] can: netlink gateway - max_hops=1
    [ 5.420865] Bluetooth: RFCOMM TTY layer initialized
    [ 5.425640] Bluetooth: RFCOMM socket layer initialized
    [ 5.430746] Bluetooth: RFCOMM ver 1.11
    [ 5.434459] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [ 5.439729] Bluetooth: BNEP filters: protocol multicast
    [ 5.444923] Bluetooth: BNEP socket layer initialized
    [ 5.449851] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [ 5.455734] Bluetooth: HIDP socket layer initialized
    [ 5.460793] 9pnet: Installing 9P2000 support
    [ 5.464929] NET: Registered protocol family 36
    [ 5.469328] Key type dns_resolver registered
    [ 5.473744] registered taskstats version 1
    [ 5.477612] Loading compiled-in X.509 certificates
    [ 5.482776] Btrfs loaded, crc32c=crc32c-generic
    [ 5.495520] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 50, base_baud = 6250000) is a xuartps
    [ 5.504539] printk: console [ttyPS0] enabled
    [ 5.504539] printk: console [ttyPS0] enabled
    [ 5.508834] printk: bootconsole [cdns0] disabled
    [ 5.508834] printk: bootconsole [cdns0] disabled
    [ 5.518146] of-fpga-region fpga-full: FPGA Region probed
    [ 5.529146] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
    [ 5.536330] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
    [ 5.543507] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
    [ 5.550689] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
    [ 5.557871] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
    [ 5.565044] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
    [ 5.572218] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
    [ 5.579398] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
    [ 5.586639] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
    [ 5.593833] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
    [ 5.601008] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
    [ 5.608178] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
    [ 5.615347] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
    [ 5.622526] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
    [ 5.629696] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
    [ 5.636872] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
    [ 5.644191] zynqmp_pll_disable() clock disable failed for rpll_int, ret = -13
    [ 5.655987] ------------[ cut here ]------------
    [ 5.660609] /axi/spi@ff050000/spidev@0x00: buggy DT: spidev listed directly in DT
    [ 5.668131] WARNING: CPU: 0 PID: 30 at drivers/spi/spidev.c:741 spidev_probe+0x164/0x1e4
    [ 5.676206] Modules linked in:
    [ 5.679256] CPU: 0 PID: 30 Comm: kworker/0:1 Not tainted 5.10.0-xilinx-v2021.1 #1
    [ 5.686726] Hardware name: xlnx,zynqmp (DT)
    [ 5.690899] Workqueue: events deferred_probe_work_func
    [ 5.696025] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)
    [ 5.702022] pc : spidev_probe+0x164/0x1e4
    [ 5.706015] lr : spidev_probe+0x164/0x1e4
    [ 5.710006] sp : ffffffc01217b7c0
    [ 5.713304] x29: ffffffc01217b7c0 x28: 0000000000000000
    [ 5.718608] x27: ffffff80402947c8 x26: 0000000000000000
    [ 5.723911] x25: ffffffc011ee23e0 x24: ffffff807cd40000
    [ 5.729214] x23: 000000000000001a x22: ffffffc011eeba08
    [ 5.734518] x21: ffffffc011eeb9e8 x20: ffffff807cd40000
    [ 5.739821] x19: 0000000000000000 x18: 0000000000000030
    [ 5.745125] x17: 0000000000000002 x16: 0000ab6e00306d64
    [ 5.750428] x15: ffffff8040275598 x14: 3030303530666640
    [ 5.755732] x13: ffffffc011e7db70 x12: 0000000000000351
    [ 5.761035] x11: 000000000000011b x10: ffffffc011ea9b70
    [ 5.766339] x9 : 00000000fffff800 x8 : ffffffc011e7db70
    [ 5.771642] x7 : ffffffc011ea9b70 x6 : 0000000000000000
    [ 5.776946] x5 : 0000000000005ff4 x4 : 0000000000000000
    [ 5.782249] x3 : 0000000000000000 x2 : 00000000ffffffff
    [ 5.787553] x1 : a9e33a2f7f802500 x0 : 0000000000000000
    [ 5.792856] Call trace:
    [ 5.795290] spidev_probe+0x164/0x1e4
    [ 5.798943] spi_drv_probe+0x80/0xe0
    [ 5.802502] really_probe+0xe8/0x4b4
    [ 5.806070] driver_probe_device+0x58/0xc0
    [ 5.810158] __device_attach_driver+0xa8/0x10c
    [ 5.814584] bus_for_each_drv+0x78/0xd0
    [ 5.818403] __device_attach+0xdc/0x17c
    [ 5.822223] device_initial_probe+0x14/0x20
    [ 5.826389] bus_probe_device+0x9c/0xa4
    [ 5.830208] device_add+0x328/0x714
    [ 5.833681] spi_add_device+0xbc/0x1b0
    [ 5.837413] of_register_spi_device+0x230/0x380
    [ 5.841935] spi_register_controller+0x7bc/0x800
    [ 5.846536] cdns_spi_probe+0x29c/0x380
    [ 5.850365] platform_drv_probe+0x54/0xb0
    [ 5.854365] really_probe+0xe8/0x4b4
    [ 5.857924] driver_probe_device+0x58/0xc0
    [ 5.862003] __device_attach_driver+0xa8/0x10c
    [ 5.866430] bus_for_each_drv+0x78/0xd0
    [ 5.870250] __device_attach+0xdc/0x17c
    [ 5.874069] device_initial_probe+0x14/0x20
    [ 5.878235] bus_probe_device+0x9c/0xa4
    [ 5.882054] deferred_probe_work_func+0x74/0xb0
    [ 5.886569] process_one_work+0x1d4/0x380
    [ 5.890569] worker_thread+0x298/0x4e0
    [ 5.894303] kthread+0x124/0x130
    [ 5.897522] ret_from_fork+0x10/0x3c
    [ 5.901088] ---[ end trace 04d6482447f4c774 ]---
    [ 5.906666] spi-nor spi0.0: SPI-NOR-UniqueID 1044003eda0b00180f00220058198125d7
    [ 5.914562] spi-nor spi0.0: trying to lock already unlocked area
    [ 5.920568] spi-nor spi0.0: mt25qu02g (262144 Kbytes)
    [ 5.926958] macb ff0d0000.ethernet: Not enabling partial store and forward
    [ 5.939436] libphy: MACB_mii_bus: probed
    [ 5.943410] macb ff0d0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0d0000 irq 38 (12:be:0b:e5:34:15)
    [ 5.953722] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
    [ 5.960311] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
    [ 5.966847] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
    [ 5.973372] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
    [ 5.980197] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 40
    [ 5.986624] i2c i2c-1: of_i2c: modalias failure on /axi/i2c@ff030000/i2c-mux@75
    [ 5.993935] i2c i2c-1: Failed to create I2C device for /axi/i2c@ff030000/i2c-mux@75
    [ 6.001605] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 41
    [ 6.007973] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1200000000 (-34)
    [ 6.016712] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1200000 KHz, changing to: 1199999 KHz
    [ 6.027504] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1200000000 (-34)
    [ 6.079565] random: fast init done
    [ 7.170834] random: crng init done
    [ 14.224196] adrv9002 spi1.0: adrv9002-phy Rev 12.0, Firmware 0.20.0.10, Stream 0.7.9.0, API version: 48.49.2 successfully initialized
    [ 14.237533] cf_axi_adc 84a00000.axi-adrv9002-rx-lpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0x00000000f846fe1e, probed ADC ADRV9002 as MASTER
    [ 14.251727] cf_axi_tdd 84a0c800.axi-adrv9002-core-tdd1-lpc: Analog Devices CF_AXI_TDD MASTER (1.00.a)
    [ 14.261568] cf_axi_tdd 84a0cc00.axi-adrv9002-core-tdd2-lpc: Analog Devices CF_AXI_TDD MASTER (1.00.a)
    [ 14.289993] cf_axi_dds 84a0a000.axi-adrv9002-tx-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A0A000 mapped to 0x00000000cabb78cf, probed DDS ADRV9002
    [ 14.321991] cf_axi_dds 84a0c000.axi-adrv9002-tx2-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A0C000 mapped to 0x00000000c62d1bb6, probed DDS ADRV9002
    [ 14.339115] of_cfs_init
    [ 14.341569] of_cfs_init: OK
    [ 14.344501] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [ 14.482491] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [ 14.489027] clk: Not disabling unused clocks
    [ 14.493506] ALSA device list:
    [ 14.496467] No soundcards found.
    [ 14.500161] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [ 14.508775] cfg80211: failed to load regulatory.db
    [ 14.509615] Freeing unused kernel memory: 2624K
    [ 14.541795] Run /init as init process
    INIT: version 2.97 booting
    Starting udev
    [ 14.672845] udevd[141]: starting version 3.2.9
    [ 14.683058] udevd[142]: starting eudev-3.2.9
    Starting tcf-agent: OK

    PetaLinux 2021.1 xilinx-uetc ttyPS0


    root@xilinx-uetc:~# cd ../..
    root@xilinx-uetc:/# ls
    bin boot dev etc home init lib log_lock.pid media mnt proc root run sbin sys tmp usr var
    root@xilinx-uetc:/# cd sys/bus/iio/devices
    root@xilinx-uetc:/sys/bus/iio/devices# ls
    iio:device0 iio:device1 iio:device2 iio:device3 iio:device4 iio:device5 iio:device6 iio:device7 iio_sysfs_trigger
    root@xilinx-uetc:/sys/bus/iio/devices# cd iio:device1
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# ls
    dev in_voltage1_bbdc_rejection_en out_voltage0_atten_control_mode_available
    frequency_hopping_hop1_signal_trigger in_voltage1_bbdc_rejection_tracking_en out_voltage0_close_loop_gain_tracking_en
    frequency_hopping_hop1_table_a in_voltage1_decimated_power out_voltage0_en
    frequency_hopping_hop1_table_b in_voltage1_digital_gain_control_mode out_voltage0_ensm_mode
    frequency_hopping_hop1_table_select in_voltage1_digital_gain_control_mode_available out_voltage0_ensm_mode_available
    frequency_hopping_hop2_signal_trigger in_voltage1_dynamic_adc_switch_en out_voltage0_hardwaregain
    frequency_hopping_hop2_table_a in_voltage1_en out_voltage0_lo_leakage_tracking_en
    frequency_hopping_hop2_table_b in_voltage1_ensm_mode out_voltage0_loopback_delay_tracking_en
    frequency_hopping_hop2_table_select in_voltage1_ensm_mode_available out_voltage0_nco_frequency
    frequency_hopping_hop_table_select_available in_voltage1_gain_control_mode out_voltage0_pa_correction_tracking_en
    in_temp0_input in_voltage1_gain_control_mode_available out_voltage0_port_en_mode
    in_voltage0_agc_tracking_en in_voltage1_hardwaregain out_voltage0_port_en_mode_available
    in_voltage0_bbdc_loop_gain_raw in_voltage1_hd_tracking_en out_voltage0_quadrature_tracking_en
    in_voltage0_bbdc_rejection_en in_voltage1_interface_gain out_voltage0_rf_bandwidth
    in_voltage0_bbdc_rejection_tracking_en in_voltage1_interface_gain_available out_voltage0_sampling_frequency
    in_voltage0_decimated_power in_voltage1_nco_frequency out_voltage1_atten_control_mode
    in_voltage0_digital_gain_control_mode in_voltage1_orx_bbdc_rejection_en out_voltage1_atten_control_mode_available
    in_voltage0_digital_gain_control_mode_available in_voltage1_orx_en out_voltage1_close_loop_gain_tracking_en
    in_voltage0_dynamic_adc_switch_en in_voltage1_orx_hardwaregain out_voltage1_en
    in_voltage0_en in_voltage1_orx_quadrature_w_poly_tracking_en out_voltage1_ensm_mode
    in_voltage0_ensm_mode in_voltage1_port_en_mode out_voltage1_ensm_mode_available
    in_voltage0_ensm_mode_available in_voltage1_port_en_mode_available out_voltage1_hardwaregain
    in_voltage0_gain_control_mode in_voltage1_quadrature_fic_tracking_en out_voltage1_lo_leakage_tracking_en
    in_voltage0_gain_control_mode_available in_voltage1_quadrature_w_poly_tracking_en out_voltage1_loopback_delay_tracking_en
    in_voltage0_hardwaregain in_voltage1_rf_bandwidth out_voltage1_nco_frequency
    in_voltage0_hd_tracking_en in_voltage1_rfdc_tracking_en out_voltage1_pa_correction_tracking_en
    in_voltage0_interface_gain in_voltage1_rssi out_voltage1_port_en_mode
    in_voltage0_interface_gain_available in_voltage1_rssi_tracking_en out_voltage1_port_en_mode_available
    in_voltage0_nco_frequency in_voltage1_sampling_frequency out_voltage1_quadrature_tracking_en
    in_voltage0_orx_bbdc_rejection_en in_voltage2_en out_voltage1_rf_bandwidth
    in_voltage0_orx_en in_voltage2_input out_voltage1_sampling_frequency
    in_voltage0_orx_hardwaregain in_voltage3_en out_voltage2_en
    in_voltage0_orx_quadrature_w_poly_tracking_en in_voltage3_input out_voltage2_input
    in_voltage0_port_en_mode in_voltage4_en out_voltage3_en
    in_voltage0_port_en_mode_available in_voltage4_input out_voltage3_input
    in_voltage0_quadrature_fic_tracking_en in_voltage5_en out_voltage4_en
    in_voltage0_quadrature_w_poly_tracking_en in_voltage5_input out_voltage4_input
    in_voltage0_rf_bandwidth name out_voltage5_en
    in_voltage0_rfdc_tracking_en of_node out_voltage5_input
    in_voltage0_rssi out_altvoltage0_RX1_LO_frequency power
    in_voltage0_rssi_tracking_en out_altvoltage1_RX2_LO_frequency profile_config
    in_voltage0_sampling_frequency out_altvoltage2_TX1_LO_frequency stream_config
    in_voltage1_agc_tracking_en out_altvoltage3_TX2_LO_frequency subsystem
    in_voltage1_bbdc_loop_gain_raw out_voltage0_atten_control_mode uevent
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode_available
    calibrated primed rf_enabled

    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# echo calibrated > in_voltage0_ensm_mode
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode_available
    calibrated primed rf_enabled
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat in_voltage0_ensm_mode
    calibrated

    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# ifconfig 192.168.1.10
    ifconfig: 192.168.1.10: error fetching interface information: Device not found
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# ifconfig eth0 192.168.1.10
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# passwd
    New password:
    Retype new password:
    passwd: password updated successfully
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test.bin > stream_config
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test.json > profile_config
    [ 238.696621] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 238.731630] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 238.765248] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)
    [ 240.241544] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 240.276558] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 240.310168] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)
    cat: write error: Invalid argument
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#

    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1# iio_info | grep iio:device
    iio:device0: ams
    iio:device1: adrv9002-phy
    [ 297.731929] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line 679, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. ARM time out .
    [ 297.760859] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001.c, in function adi_adrv9001_Temperature_Get, in line 556, variable name NULL.Error message ArmCmdStatusWait() failed due to thrown ARM error. ARM time out .
    [ 297.789000] adrv9002 spi1.0: adrv9002_phy_read_raw_no_rf_chan, 1809: failed with "ArmCmdStatusWait() failed due to thrown ARM error. ARM time out " (3)
    [ 297.802802] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Get, in line 963, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 297.832417] adrv9002 spi1.0: adrv9002_attr_show, 571: failed with "Frequency hopping not enabled in device profile" (3)
    [ 297.843338] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Get, in line 963, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 297.872950] adrv9002 spi1.0: adrv9002_attr_show, 571: failed with "Frequency hopping not enabled in device profile" (3)
    [ 299.968781] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_Cmd_Write, in line 774, variable name device.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
    [ 299.996502] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_Configuration_Inspect, in line 623, variable name NULL.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
    [ 300.024906] adrv9002 spi1.0: adrv9002_fh_config_dump_show, 936: failed with "ARM Mailbox Busy. Command not executed in ArmCmdWrite()" (3)
    [ 300.037456] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 300.068208] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
    [ 300.095320] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
    [ 300.107000] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 300.137756] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
    [ 300.164849] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
    [ 300.176611] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 300.207367] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
    [ 300.234478] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
    [ 300.246173] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect_Validate, in line 413, variable name devStateInfo->frequencyHoppingEnabled.Error message Frequency hopping not enabled in device profile.
    [ 300.276927] adrv9002 spi1.0: [ERROR]: Error number 3 (0x00000003), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_fh.c, in function adi_adrv9001_fh_HopTable_Inspect, in line 863, variable name NULL.Error message Frequency hopping not enabled in device profile.
    [ 300.304036] adrv9002 spi1.0: adrv9002_hop_table_dump_show, 993: failed with "Frequency hopping not enabled in device profile" (3)
    iio:device2: axi-adrv9002-rx-lpc (buffer capable)
    iio:device3: axi-adrv9002-rx2-lpc (buffer capable)
    iio:device4: axi-core-tdd (label: axi-core-tdd-1)
    iio:device5: axi-core-tdd (label: axi-core-tdd-2)
    iio:device6: axi-adrv9002-tx-lpc (buffer capable)
    iio:device7: axi-adrv9002-tx2-lpc (buffer capable)
    root@xilinx-uetc:/sys/bus/iio/devices/iio:device1#

  • Hi,

    Well, the versions are ok. Can you share the profiles you're trying to load?

    - Nuno Sá

  • Hii ,
           I have uploaded the profile files on the git-hub , Please find the link below . there is all profile files which we had tried.

    https://github.com/sagarvvdn/Query/blob/main/adrv%20test.zip

  • Hi,

    You said you have the device clock set as 40MHz... In profiles 1 and 2 I see it as 38.4MHz which probably won't work. Anyways, I will be able to only test the profiles with 38.4MHz. I'll try to test it on my side tomorrow morning....

    - Nuno Sá

  • Hii ,
          We have tested the  both frequency 38.4 MHz and 40 MHz on the board.
          In the folder both type of profile files are available set-3,5,6  has 40 Mhz and set-1,2,4 has  38.4 MHz files.

  • Hi,

    I just tested your 38.4MHz profiles on ZCU102 with the evaluation board.

    https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp

    The profiles load without errors.

    Do you think it's useful to you if I would provide the ZCU102 boot files I used for testing?

    -Michael 

  • Hii michael ,
                         We have already tested these files  with ZCU102 evaluation board , its working in eval board, but our main concern is that we are  facing issue while uploading in our  customised board , We are not able to identify the reason why this error is coming during the profile file upload.  Also i wanna  share with you  we are using single-ended clock  in our customised ADRV RF board . i have  already attached the  schematic in this thread, in which single ended  connection mentioned .i am attaching  the log error again.


    xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.bin > stream_config
    xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.json > profile_config
    [ 3698.162265] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3698.197278] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3698.230896] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)
    [ 3699.598724] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3699.633727] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3699.667339] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)


    Also i have checked the  clock and power , both are okay .

Reply
  • Hii michael ,
                         We have already tested these files  with ZCU102 evaluation board , its working in eval board, but our main concern is that we are  facing issue while uploading in our  customised board , We are not able to identify the reason why this error is coming during the profile file upload.  Also i wanna  share with you  we are using single-ended clock  in our customised ADRV RF board . i have  already attached the  schematic in this thread, in which single ended  connection mentioned .i am attaching  the log error again.


    xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.bin > stream_config
    xilinx-uetc:/sys/bus/iio/devices/iio:device1# cat /tmp/test1.json > profile_config
    [ 3698.162265] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3698.197278] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3698.230896] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)
    [ 3699.598724] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure_Validate, in line 39, variable name readPattern.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3699.633727] adrv9002 spi1.0: [ERROR]: Error number 1 (0x00000001), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_powermanagement.c, in function adi_adrv9001_powermanagement_Configure, in line 70, variable name NULL.Error message ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board.
    [ 3699.667339] adrv9002 spi1.0: adrv9002_power_mgmt_config, 2597: failed with "ARM memory is not accessible. Check whether device clock and/or power is connected to the ADRV9001 board" (1)


    Also i have checked the  clock and power , both are okay .

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.