KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi all,
we are using the 7z035+adrv9001 custom board (not the zc705 or the zcu102 evaluation boards) whose image/kernel is originated from the petalinux platform ( which derived from this fact cannot be connected tp the TES SW ) .
in this days we are using the TES version Argo Navis 0.18.1.
before we update the TES version to the current one we were able to load the json and bin file (for the profile ) to the board using this two commands(in the order which shown below):
cat /home/root/<name of bin file>.bin > /sys/bus/iio/devices/iio:device0/stream_config
cat /home/root/<name of bin file>.json > /sys/bus/iio/devices/iio:device0/profile_config
But now with the TES version Argo Navis 0.18.1 we cant load the profile correctly (which result with iio devices which initialized correctly )
what is the problem and how can we solve it?
with best regards.
Dror & Raz
__CommunityServer__Service__ - Moved from TES GUI & Software Support ADRV9001 – ADRV9007 to Design Support ADRV9001 – ADRV9007. Post date updated from Wednesday, December 22, 2021 11:20 AM UTC to Thursday, January 22, 2026 10:48 PM UTC to reflect the move.
Hi Dror & Raz,
As this is the start of the Holiday period I cannot currently move this question to the relevant forum but I will do so as soon as I can.
This question will get better support on the Linux SW Drivers forum as it may be a version issue with the Linux drivers you are using.
Regards
Hello Dror & Raz,
The issue here is likely due to version mismatch. SDK v0.18.1 was the most recent release at the time of posting this question (we are now on SDK v0.19). The Linux SW always lags behind the product line SDK by a few releases, so APIs that have been implemented, activated or redesigned in SDK v0.18.1 will not work in the Linux SW for some time. How much time this will take is beyond our control, as we do not support the Linux SW in the product line team. The biggest change that comes to mind with v0.18.1 is the addition of Dynamic Profile Switching, which I can certainly understand causing issues for loading profiles with the Linux SW.
As such, I'm afraid your options are rather limited. You can revert to the previously working revision of SDK and continue development as far as possible before migrating to the latest SDK revision, or you could ask the Linux forum when they expect to support the latest APIs as of SDK v0.18.1.
At present, that's the best advice I can offer. I'll ask around if anyone has any visibility on when this mismatching issue should be resolved, but I would suggest asking the Linux forum when they expect to support the v0.18.1 APIs. Do let me know if there's anything else we can help with.
Best Regards,
Oisín.
HI,
Can you explain how you added json profile to your petalinux image