I have a question regarding the 2 RF Synthesizers in the ADRV9002 for which there is not sufficient detail in the datasheet nor the ADRV9001 System Development User Guide.
There is only mention that this is a fractional-N synthesiser with no detail on the resolution of the fraction. In addition there is also no detail on the limits of the reference frequency at the phase detector input nor on the reference divider divide range if any divider is used.
I have an application that I do not intent to run from a 38,4MHz device clock, but my own custom clock, but there is insufficient details in the above mentioned documentation to ascertain my design will work as intended. I need to verify that I can achieve my channel spacing too with my custom clock.
Can info be provided with some more basic details on the RF Synthesizers so as to ensure that I can achieve for what I need in my final application.
A similar situation arises for the Clock Synthesizer that ultimately determines the sampling rate.
Thank you.