Post Go back to editing

channel configuration in ADRV9002 while changing internal LO

Hi ,

As mentioned in the user guide UG-1828  is  - "when changing the LO, user needs to make sure all channels that utilize the LO is configured. For example, if Tx1 and Rx1 are using LO1, and user wants to change LO1, then user needs to configure both Tx1 and Rx1 to achieve that. If all channels (Tx1 Tx2 Rx1 Rx2) are using the same LO, and user needs to change the LO, then user needs to configure all channels (Tx1 Rx2 Rx1 Rx2) to achieve that."

 Here what is meant by "configuring  both Tx1 and Rx1 while changing LO "which configuration we need to take for TX1 and Rx1. please elaborate or clarify.

regards,

manideep