Post Go back to editing

ADRV9002 FH-TDD solutions

Thread Summary

The user inquires about implementing a TDD system with Frequency Hopping using the ADRV9002, without a predefined sequence of Tx/Rx frames. The final answer indicates that the automated TDD state machine timings are fixed post-initialization, and suggests designing a custom state machine for the platform to achieve the desired random frame switching. The custom state machine can control the Hop and Enable signals manually, aligning with the TDD enablement delays and DMA triggers.
AI Generated Content

Hello ADI Team,

We want to implement using an ADRV9002 a TDD system with Frequency Hopping but without having a predefined repeatable sequence of Tx/Rx frames. In other words, we want to set the next HOP frame to Rx or Tx in a random way.

  1. If we use the automated TDD, is it possible and how to change the RX/Tx Pins and Rx/Tx DMA asserts on the fly?
  2. If Not, we have to implement two separate frames, one frame for Rx and one frame for Tx, so we can configure the next automated TDD frame while the current is on. 
    1. Is a solution like this possible, to configure the next automated TDD frame while the current is on?
    2. In the structure adi_fpga9001_TddFrameTiming_t, If we set the frameStartTrig to ADI_FPGA9001_TDD_TRIGGER_GPIO instead of ADI_FPGA9001_TDD_TRIGGER_IMMEDIATE, how to assign a GPIO to trigger the automated TDD Enable?
  3. If we don’t use the automated TDD but we take advance of Tx/Rx Enables and Hop Pin GPIO,
    1. what is the best way to trigger the Tx/Rx DMAs in order to align with the TDD Enablements Delays?
    2. How to assign a GPIO to trigger the Tx/Rx DMA?
  4. Could you advise other solutions?

Thanks in advance.

gstou

  • Hello gstou,

    You present us with an interesting use-case, however it certainly is possible to support your application.

    The Automated TDD state machine that we provide as part of our SDK and TES implementations can be used to go from evaluation of the product all the way through to production, however it is always important to note that the Auto TDD State Machine exists on the FPGA, not on the device. While using our Eval setup (eval board and ZC706 or ZCU102) you can use the automated TDD feature to evaluate the products performance under auto TDD, as well as determine device timing requirements.

    However, when migrating to your own custom platform, you're free to design your own Auto TDD state machine however you wish. If you write custom code to handle this custom state machine, your own APIs can be integrated with our own (not by modifying our SDK, only by modifying our produced sample code from TES). This method gives you complete control of the state machine's behavior, freeing you from the constraints put in place in our software. It's certainly not a trivial undertaking, but for your application it will probably yield the most satisfactory results.

    To answer your questions about our Auto TDD state machine:

    1. No, I'm fairly certain our state machine timings are fixed after initialization.
    2. Again no, after initialization our TDD frames are fixed. As for assigning a GPIO pin to the autoTDD enable, I'm actually not certain. I've never seen this done nor heard of an application that needed it. I don't believe it makes the most sense either, as the autoTDD enable signal exisits on the FPGA platform, not on the device. Using the device to control it is similar to getting the platform to tell the device to tell the platform to enable auto TDD, which is a very roundabout way of doing it.
    3. Handling enablement delays is among the harder parts of designing state machine timings. We provide two different guides on how to approach this issue:
      https://ez.analog.com/wide-band-rf-transceivers/tes-gui-software-support-adrv9001-adrv9007/w/documents/15627/automated-tdd
      https://www.youtube.com/watch?v=huufF5c_hOY&t=1s
      As to your second question, there's no real reason why you use a GPIO pin to control a DMA signal. The DMA is the control of data transfer to and from the platform. Essentially it's a second enable signal that you can use to avoid blank or useless data from being sent over Tx or read over Rx. It is essential to note that this signal is a platform signal, not a device signal. Just like before, using a GPIO to control this would be like telling the platform to tell the device to tell the platform when it should exchange data. Does this make sense?
    4. For the reasons outlined above, it may be best to explore building your own state machine for your platform. You can experiment using the Eval platform, FH doesn't rely on Auto TDD to operate. once your desired setup is programmed, with hop tables loaded, you can control the Hop signal and the Enable signals manually, which also means you can design a block of code to control them for you.

    I understand that I'm recommending a fairly large undertaking, but I do believe that investing in this custom state machine will lead to the best results for your application, rather than attempting to circumvent the limitations of our SW. Do let me know if you have any further questions in the meantime!

    Best Regards,
    Oisín.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.