Hello
our customer is evaluating ADRV9002NP/W1/PCBZ Silicon revision B0.
They use TES v.0.15 as v.0.16 is not compliant with Silicon revision B0.
There are a couple of questions to the transmitted signal.
in the attached document you may find screen shots.
Could you please clarify:
- The given frequency Tx does not coincide with the real one (it is seen in all figures). We have to adjust its Freq offset. Why is this happening?
- In Figure 3, with a wide bandwidth, it can be seen that in addition to the unmodulated carrier, numerous harmonics are present in the spectrum. What's the matter?
- In the case of a modulated signal (Fmod = 0), numerous combinatorial frequencies appear in the spectrum - Fig. 4. In addition, in Fig. 4, an increased level of phase noise is observed when approaching the carrier.
- Figures 5 and 6 - where does the parasitic AM come from? The modulation frequency is approximately 23.6 kHz.
- At Fmod = 1 kHz, the emission spectrum is very noisy (Figures 8 - 10).
- Similar questions arise when considering a dual frequency signal (Figures 11 - 16).
Regards
Evgeny

Figure 1.