Post Go back to editing

SDK Code for ADRV9002 does not seem to enable the user RX filter.

I have a custom RF filter that I loaded into the TES.

The filter is correct in the TES.

I then used the TES to output C code.

I see the filter coefficients in the created file initialize.c and the coefficients are correct and placed in the variable init_pfirBuffer_pfirRxWbNbChFilterCoeff_A_5.

I only have one receiver enabled in TDD mode in the TES.

The filter does not seem to be used.

When I plot the fft of the data, the data is not being filtered.

How do I enable this?

Note that the other parameters in initialize.c are being set correctly.

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.