ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi,
What is the resolution of DAC of ADRV9002?
The high-performance ADC is 5bits, and low Σ-Δ ADC is 16bits described in UG-1828.
Regards,
HM
Hi HM,
To begin answering your question, I need to correct your second statement: The high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC). The low-power ADC is a 16-bit Voltage Controlled Oscillator (VCO) architecture.
As for the DACs, I'm assuming you mean the DACs present on the Tx datapath? These are 16-bits wide (Please review TRANSMITTER SIGNAL CHAIN - ANALOG FRONT END (AFE) - DAC in the user guide for more details), however there are also Auxiliary DACs/ADCs which are 12-bits wide (please review AUXILIARY CONVERTERS AND TEMPERATURE SENSOR in the user guide for more details)
Thanks,
Oisín.
If the high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC), Then what will be typical SNR performance for the 40MHz Bandwidth?
Is it 5 bit or 16-bit? Pls confirm.
If the high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC), Then what will be typical SNR performance for the 40MHz Bandwidth?
Is it 5 bit or 16-bit? Pls confirm.
Hi Sugu,
In the user guide under Rx/ORx Signal Chain - Receive Data Chain: Analog Front End there is a section dedicated to the ADC options. Here it describes each ADC option in more detail, but in answer to your question I can confirm that the HP ADC is a 5-bit CTDS ADC, the LP ADC is a 16-bit VCO ADC.
I don't have the exact data you're requesting, I'll look into it over the coming days. In the datasheet under Receiver Specifications there is a host of measurements going through Noise Figure, Image Rejection, etc. across center frequency. Let me know if this data answers your questions.
Regards,
Oisín.