ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi,
What is the resolution of DAC of ADRV9002?
The high-performance ADC is 5bits, and low Σ-Δ ADC is 16bits described in UG-1828.
Regards,
HM
Hi HM,
To begin answering your question, I need to correct your second statement: The high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC). The low-power ADC is a 16-bit Voltage Controlled Oscillator (VCO) architecture.
As for the DACs, I'm assuming you mean the DACs present on the Tx datapath? These are 16-bits wide (Please review TRANSMITTER SIGNAL CHAIN - ANALOG FRONT END (AFE) - DAC in the user guide for more details), however there are also Auxiliary DACs/ADCs which are 12-bits wide (please review AUXILIARY CONVERTERS AND TEMPERATURE SENSOR in the user guide for more details)
Thanks,
Oisín.
Hi HM,
To begin answering your question, I need to correct your second statement: The high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC). The low-power ADC is a 16-bit Voltage Controlled Oscillator (VCO) architecture.
As for the DACs, I'm assuming you mean the DACs present on the Tx datapath? These are 16-bits wide (Please review TRANSMITTER SIGNAL CHAIN - ANALOG FRONT END (AFE) - DAC in the user guide for more details), however there are also Auxiliary DACs/ADCs which are 12-bits wide (please review AUXILIARY CONVERTERS AND TEMPERATURE SENSOR in the user guide for more details)
Thanks,
Oisín.
Hi, Oisin,
Thank you for your support.
I understand the DAC resolution.
I made a mistake in the description of ADC. Thank you for correcting it.
I have another question.
What kind of architecture is the VCO architecture of the LP ADC?
Thanks,
HM
Hi HM,
VCO based ADC's are a particular type of ADC which are designed to be highly digital in nature. This architecture is very useful for on-chip testing and integration into CMOS systems. VCOs themselves are a standard piece of electronics, they output a digital square wave whose frequency is a function of the input voltage. By comparing the output frequency to that of a separate clock reference using digital counters, one can create an all-digital ADC. These circuits are generally liked for their ability to implement simplified versions of high-order Sigma-Delta ADC's, which come with great noise characteristics and a very high dynamic range. Despite the LP ADC's on the ADRV9002 Rx datapath having slightly worse performance than the HP ADC's, you will note that they do have a very large dynamic range and great noise performance.
Unfortunately I struggled to find an article on analog.com which discussed this circuitry, however a quick Google search returned numerous books, papers and articles which discuss this architecture in varying degrees of depth. Here's one block diagram I found of this architecture, available at the following link: https://www.google.com/search?q=VCO+ADC+images&rlz=1C1CHBF_enIE861IE861&sxsrf=ALeKk01ZWgLO9htcJXozFzHpELLDhuVC3Q:1598273010429&source=lnms&tbm=isch&sa=X&ved=2ahUKEwjDpqn47rPrAhVJQxUIHZMaBGAQ_AUoAXoECAwQAw&biw=1920&bih=1089#imgrc=pchazMk5Eb4mgM

I do hope this helps. Thanks very much for your interest.
Best Regards,
Oisín.
Hi, Oisin,
Tahnk you for your useful information.
Regards,
HM
If the high-performance ADC is a 5-bit Continuous Time Delta Sigma ADC (CTDS ADC), Then what will be typical SNR performance for the 40MHz Bandwidth?
Is it 5 bit or 16-bit? Pls confirm.
Hi Sugu,
In the user guide under Rx/ORx Signal Chain - Receive Data Chain: Analog Front End there is a section dedicated to the ADC options. Here it describes each ADC option in more detail, but in answer to your question I can confirm that the HP ADC is a 5-bit CTDS ADC, the LP ADC is a 16-bit VCO ADC.
I don't have the exact data you're requesting, I'll look into it over the coming days. In the datasheet under Receiver Specifications there is a host of measurements going through Noise Figure, Image Rejection, etc. across center frequency. Let me know if this data answers your questions.
Regards,
Oisín.