Post Go back to editing

Make a new SD card for the ADRV9002 SDK

Thread Summary

The user's SD card for the ZC706 and ADRV9002 got corrupted. A step-by-step guide to re-image the SD card using SDK 13 or higher is available on the Analog Devices EngineerZone. The original SD card image for the ZC706 and ADRV9002 is not publicly available, but the SW team has fixed the download issue for the ZCU102 / ADRV9002 image. For manual SD card imaging, ensure the .zip file is not corrupted or incomplete.
AI Generated Content

My SD card got corrupted.

Where do I go to make a new SD card that will work for the ZC706 and the ADRV9002?

I want to make sure I duplicate the same SD card that came with the board.

Thanks

Charly

Edit Notes

fixed the fpga board name
[edited by: charlyelkhoury at 1:13 PM (GMT -4) on 19 Aug 2020]

Thread Notes

Parents Reply
  • Hi Yasin,

    I'm afraid this is not a service we provide. It is however possible to download the SD card image using our imaging software and then write it manually to an SD card, so if needed you could download the image on a separate machine and compress and email it to the workstation PC.

    Best Regards,

    Oisín.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.