Post Go back to editing

Make a new SD card for the ADRV9002 SDK

Thread Summary

The user's SD card for the ZC706 and ADRV9002 got corrupted. A step-by-step guide to re-image the SD card using SDK 13 or higher is available on the Analog Devices EngineerZone. The original SD card image for the ZC706 and ADRV9002 is not publicly available, but the SW team has fixed the download issue for the ZCU102 / ADRV9002 image. For manual SD card imaging, ensure the .zip file is not corrupted or incomplete.
AI Generated Content

My SD card got corrupted.

Where do I go to make a new SD card that will work for the ZC706 and the ADRV9002?

I want to make sure I duplicate the same SD card that came with the board.

Thanks

Charly

Edit Notes

fixed the fpga board name
[edited by: charlyelkhoury at 1:13 PM (GMT -4) on 19 Aug 2020]

Thread Notes

Parents Reply Children
No Data