Post Go back to editing

Make a new SD card for the ADRV9002 SDK

Thread Summary

The user's SD card for the ZC706 and ADRV9002 got corrupted. A step-by-step guide to re-image the SD card using SDK 13 or higher is available on the Analog Devices EngineerZone. The original SD card image for the ZC706 and ADRV9002 is not publicly available, but the SW team has fixed the download issue for the ZCU102 / ADRV9002 image. For manual SD card imaging, ensure the .zip file is not corrupted or incomplete.
AI Generated Content

My SD card got corrupted.

Where do I go to make a new SD card that will work for the ZC706 and the ADRV9002?

I want to make sure I duplicate the same SD card that came with the board.

Thanks

Charly

Edit Notes

fixed the fpga board name
[edited by: charlyelkhoury at 1:13 PM (GMT -4) on 19 Aug 2020]

Thread Notes

Parents Reply
  • Hi Charly,

    There should be 2 SD cards in the kit you have. Do you not have 2? It's also advisable to backup the SD card image in some way if you can, like on your laptop or PC. Given the nature of the contents of the SD card there's quite a lot of red tape to go through before we can make the image publicly available, and as such it currently isn't publicly available.

    If you don't have the spare SD card, or any other saved copy of the image, then we may need to figure out some other solution.

    Thanks,

    Oisín.

Children