Post Go back to editing

GUI connection issue

Thread Summary

The user encountered connection issues with the ADRV9002 evaluation board using the TES software. The final solution involved checking the FPGA configuration and the ADP5056 power supply chip. The ADP5056 enable pin was found to be high, but the output voltages were incorrect, suggesting potential damage to the ADP5056. The user plans to contact an agent for further assistance.
AI Generated Content

I have trouble connecting to the board using the evaluation software (TES). Getting GUI pop-up error.

Thread Notes

Parents
  • Hello,
    I have also connection problems. ADRV9002 + ZYNQ702



    The directory /home/analog/adrv9001_server/resources/Adi.Adrv9001.Server/
    contains Adrv9001Server_B0_29.2.0


    Ping in both directions is ok.

    How can I star the server manualy?

    Best regards
     Stefan

  • Hi Stefan,

    You can manually start the server by navigation to that 'Adi.Adrv9001.Server/' folder and then running:

    ./Adrv9001Server_B0_29.2.0

    This should manually start the server. While the server is starting it will attempt to connect to the ADRV9002 device. If this connection attempt fails then the server will fail, so make certain the device is connected securely and operational. If the server starts successfully the command prompt indicate that the server is waiting for something to connect to it. At this point go to TES on your host laptop and connect to the platform. If TES connects you should be good to go, it'd be unlikely that you'll need to perform this step again.

    If you continue having issues capture a screenshot of the command prompt output and post it here, we'll take a look at it and provide next steps.

    Best Regards,

    Oisín.

Reply Children
No Data