| SLA Status | Assignee | Support Status |
|---|---|---|
| ⚠ 4784 hours | Open | |
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
Hello,
We are working with the ADRV9371, but we get an issue when we try to communicate by the SPI. We use the Xilinx SPI IP on a VCU108, with a Micro blaze MCU to implement the Mykonos code.
We put both Resetb and FMC_clk_resetb to one, and we have something coming out from the FPGA SPI, we checked it with a probe and everything is going through the FMC connector as it should be.
But at the moment we can’t get any response coming back from the Analog device board, but it’s working with the TES software on a ZC706. We compared the frame shape and they match (clock polarity and phases are good).
Best regards.
__CommunityServer__Service__ - Moved from TES GUI & API Software Support AD9371/AD9375 to Support AD9371/AD9375. Post date updated from Monday, April 24, 2017 5:15 PM UTC to Friday, January 30, 2026 12:11 AM UTC to reflect the move.
Are you running the same project on ZC706+AD9371 evaluation board?
Hope you are taking care of VADJ voltage which comes from FPGA through which VDD_IF voltage is supplied to AD9371 board, below screenshot from schematics
Are you running the same project on ZC706+AD9371 evaluation board?
Hope you are taking care of VADJ voltage which comes from FPGA through which VDD_IF voltage is supplied to AD9371 board, below screenshot from schematics
I had the problem of "the AD9371 SPI port is dead" on the Eval Board.
The problem appears to be that the reset logic is flaky, and if you just use a 10k pull-up, the !reset line goes high before the power has stabilized.
I found that the act of adding a test lead added enough capacitance for it to work 50% of the time. AFAIK, some kind of manual reset is needed.
Kind of unfortunate that the "Evaluation Board" has this bug. . .
There is no bug with the eval board reset. The eval board was released few years back and this is the first time we hear an issue with reset.
Reset not proper should not damage the SPI interface.
Reset is pulled up with 10K to 1.8V VDD_IF voltage and this voltage will come up after all the supplies are brought up .
In any case , because of the reset pin SPI interface doesn't go bad and no customers have reported this issue earlier .
Was this board working before and what change caused this failure ?