i have configured the AD9373 to 2GHz Frequency.
programed the TX/RX/Sniffer LOs. and configured as internal LO.
once the Device programed the LO leakage at the port is -36dBm.
i have gone to the Transmitter page on GUI and found when i change the attenuation to 10dB.
the Output noise goes down, but the LO power increased by 10dB.
do we need to calibrate the path every time we sett the attenuator?? i dint expected that the TX attenuator will change the LO leakage in opposite direction.
Please clarify............