Post Go back to editing

AD9375 has BW minimum of 8 MHz in the Rx that would limit the sensitivity of the receiver. Now if I am interested to use it for 1.4MHz LTE signal how can I make sure that the receiver can sense this ?

For AD9371/AD9375  :

Lets say I have a Receiver with minimum bandwidth of 8 MHz .

For LTE the minimum BW is 1.4 MHz .

 

So is it right to say the minimum detectable signal of the receiver will not be able to detect the LTE 1.4 MHz and 5 MHz BW since it is below the noise floor of the RX?

or , is there a way I can use the RX to detect the 1.4MHz band.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.