Post Go back to editing

AD9371 + ZU15EG: Intermittent SYSREF Alignment Error Despite Integer LMFC/SYSREF Relationship

Category: Software
Product Number: AD9371
Software Version: vivado 2018.3 , sdk 2018.3

Hello , 

I am working on a custom AD9371 + ZU15EG design and am seeing the "SYSREF Alignment Error = Yes" status intermittently after some power cycles. Most power-ons work correctly, but occasionally the alignment error is reported.
Iam using reference project HDL and NO OS project provided in ADI github.

I reviewed the ADI JESD troubleshooting documentation and found two possible causes:

SYSREF frequency is not an integer multiple/submultiple of the LMFC frequency
SYSREF violating setup/hold timing with respect to the JESD device clock

For our configuration:

Lane rate = 2457.6 Mbps
F = 2 octets/frame
K = 32 frames/multiframe
LMFC frequency = 3.84 MHz
SYSREF frequency = 0.96 MHz

Since SYSREF = LMFC/4, the first condition appears to be satisfied.

Regarding the second point, the troubleshooting guide suggests constraining the SYSREF path relative to the device clock. We would like to investigate this further.

Our clocking setup is as follows:

HMC7044 generates both clocks and SYSREF.
Clock and SYSREF traces are length matched on the PCB.
AD9371 reference clock = 122.88 MHz.
We are using the standard 61.44 MHz profile configuration files from the ADI reference design.
In the HDL reference design, the JESD device clock is generated by a Clock Wizard whose input is the GT Channel 0 output clock, and the Clock Wizard output is used as the device clock for the JESD IP.

My questions are:

In this architecture, what clock should be used as the timing reference when constraining the SYSREF path?
How should the SYSREF path be constrained in Vivado?
Has anyone observed intermittent SYSREF alignment errors in a similar AD9371 setup despite having matched clock/SYSREF routing?
Besides SYSREF frequency relationship and setup/hold timing, are there any other common causes that could lead to intermittent SYSREF alignment errors across power cycles?

Any guidance or recommendations would be greatly appreciated. Thanks.

Parents
  • SYSREF needs to be source synchronous with the device clock and is usually generated together with the device clock by a clock generation chip (HMC7044). The sysref must meet setup and hold timing to device clock. Also ensure that the SYSREF and DEVCLK trace lengths are matched.

    There is a possibility that the issue would be related to SYSREF setup/hold timing.

    We would need to meet the AD9371 datasheet specified Setup/hold timings, capture the SYSREF setup/hold timings.

    We would recommend posting the Vivado related /FPGA queries in the below forum.

      FPGA Reference Designs 

Reply
  • SYSREF needs to be source synchronous with the device clock and is usually generated together with the device clock by a clock generation chip (HMC7044). The sysref must meet setup and hold timing to device clock. Also ensure that the SYSREF and DEVCLK trace lengths are matched.

    There is a possibility that the issue would be related to SYSREF setup/hold timing.

    We would need to meet the AD9371 datasheet specified Setup/hold timings, capture the SYSREF setup/hold timings.

    We would recommend posting the Vivado related /FPGA queries in the below forum.

      FPGA Reference Designs 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.