I am currently working with the AD9371 transceiver and would like to implement a receive-only (RX-only) configuration for my application. My setup does not require any transmission functionality.I only need to capture and process incoming RF signals.
I am using the AD9371 RF transceiver with the Xilinx ZC706 evaluation board. The connection between the ZC706 and AD9371 is made via the standard FMC interface. The reference design used is based on ADI's No-OS framework, built and programmed using Xilinx Vivado and Vitis tools.