Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Sampling Rate Constraints of AD9371 on ZC706 and High-Speed RF Board Options

Category: Hardware
Product Number: AD9371

I'm working on an AD9371 and ZC706 No-OS application with a fixed device clock of 122.88 MHz, and I observe a limited range of achievable sampling rates, from 49.152 MHz up to 307.2 MHz. Could you clarify what factors restrict the AD9371’s sampling rate on the ZC706 board to a range of approximately 30 MSPS to 320 MSPS?

Are these limitations due to hardware constraints of the ZC706, the AD9371 transceiver, or a combination of both?

Additionally, which RF boards would support sampling rates higher than 500 MSPS?

Edit Notes


[locked by: srimoyi at 12:29 PM (GMT -5) on 15 Nov 2024]

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.