Post Go back to editing

ZCU102+AD9371

Thread Summary

The user is new to programming and wants to implement a frequency measurement algorithm using ZCU102 and AD9371. They encountered an issue connecting the board with TES GUI, showing 'Platform problem: algorithm negotiation failed'. The solution is to use the Windows-based TES GUI SD Card for proper evaluation. Alternatively, the user can use Linux-based drivers and the IIO oscilloscope GUI to read ADC data from RX1 and RX2, where voltage 0 corresponds to RX1 and voltage 1 to RX2.
AI Generated Content
Category: Hardware
Product Number: AD9371
Software Version: 2017.4

hi all, i have ZCU102+AD9371, i am new to Programming and want to learn and implement frequency measurement algorithm. share if any links or docs for quick start.

thanks in advance.

Thread Notes

Parents Reply Children
No Data