| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Missed after 256 hours |
vanitha |
Closed |
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
hi all, i have ZCU102+AD9371, i am new to Programming and want to learn and implement frequency measurement algorithm. share if any links or docs for quick start.
thanks in advance.
Dorant - Moved from RF and Microwave to TES GUI & API Software Support AD9371/AD9375. Post date updated from Saturday, November 9, 2024 11:25 AM UTC to Thursday, November 14, 2024 2:43 PM UTC to reflect the move.
__CommunityServer__Service__ - Moved from TES GUI & API Software Support AD9371/AD9375 to Support AD9371/AD9375. Post date updated from Thursday, November 14, 2024 2:43 PM UTC to Friday, January 30, 2026 12:15 AM UTC to reflect the move.
Not sure what's the question here.
We have lot of details wrto programming the chip in UG-992 , you may refer from page14.
We support the queries related to AD9371 here and your question is outside of our scope
I am trying to interface AD9371 with ZCU102 Eval Board, i want read ADC data from AD9371 through ZCU102, provide if any sources available.
And also Provide, which ports to be used for reading ADC data on FMC Connector.

PFA FYI
We can analyse the RX data by saving the I/Q data from the "Receive Data" tab in the TES GUI(Floppy disk icon in the below figure).
For more details, refer to "Receiver Setup" section in the UG-992 (page 305).

Download the TES GUI from the below link.
https://www.analog.com/en/lp/001/transceiver-evaluation-software.html
I not able to connect Board with TES, showing following error
"Platform problem: algorithm negotiation failed"
Are you using eval board or custom board? TES GUI connects only with our EVB platform.
Which SD card are you using ? We have two SD-Cards given with the board ,use the one with 'Windows based TES/ ADRV9371-SDCARD' on it.

Please follow TRANSCEIVER EVALUATION SOFTWARE section from UG-992 about how to get started with the TES GUI and how to configure the AD9371 TES GUI .Place the SW11 toggle switches in the positions as shown in the below figure (Toggle Switch 1, Toggle Switch 2, and Toggle Switch 5 = Position A.

Once you power on Is the board booting? LED will blink in sequence until boot is completed.
Also please refer to the below troubleshooting guide for issues related to TES connection.
i am using zcu102 eval board, but i am not having Windows based TES/ ADRV9371-SDCARD, but i could able to boot the board without any errors with kuiper linux SD Card.
We should be using Windows based TES GUI SD Card to work with TES GUI, else it won't work.
Okay, i will check by using Windows based TES GUI SD Card. what will be the alternate solution if we don't use that SD carḍ.
i am a beginner...
parallelly, I'm trying to build interface block for AD9371 with zcu102 in Vivado. please check attached pic.
which ports I have to use for reading ADC data of Rx1 & RX2 from AD9371
i am a beginner...
parallelly, I'm trying to build interface block for AD9371 with zcu102 in Vivado. please check attached pic.
which ports I have to use for reading ADC data of Rx1 & RX2 from AD9371
Okay, i will check by using Windows based TES GUI SD Card. what will be the alternate solution if we don't use that SD carḍ.
For evaluating using TES GUI, you need to use windows based sd card.
You can also use Linux based drivers and use the IIO oscilloscope GUI for evaluating. You will be able to see the captured data on RX using this GUI.
Download the image and the GUI application from the below links:
https://wiki.analog.com/resources/tools-software/linux-software/kuiper-linux
https://wiki.analog.com/resources/tools-software/linux-software/iio_oscilloscope
hi,
i am able to see only voltage0_i, voltage0_q, voltage1_i, voltage1_q.
how to check Rx channels data in IIO oscilloscople
Voltage 0 refers to RX1 and voltage 1 refers to RX2 data. Refer below link:
https://wiki.analog.com/resources/tools-software/linux-software/iio_oscilloscope
okay, i will check
hi,
this thread can be closed.
regards,