| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 2 hours |
Closed | |
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
I am currently working with the AD9371 RF transceiver and using either the Transceiver Evaluation Software (TES) or the AD9371 FilterWizard application for a No-OS application. I need to configure the sampling rates for both the Tx and Rx paths.
Could someone provide me with the maximum and minimum sampling rates that can be configured for Tx and Rx using these tools or is there any other tools where I can configure the minimum sampling rate less than 50MHz and above 500MHz?
Specifically:
If there are any additional considerations or constraints when setting these rates, such as specific configurations or limitations based on the sampling rate, I would appreciate that information as well.
Thank you in advance for your help!
__CommunityServer__Service__ - Moved from TES GUI & API Software Support AD9371/AD9375 to Support AD9371/AD9375. Post date updated from Friday, September 13, 2024 1:23 PM UTC to Friday, January 30, 2026 12:13 AM UTC to reflect the move.