| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 2 hours |
Closed | |
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
I am currently working with the AD9371 RF transceiver and using either the Transceiver Evaluation Software (TES) or the AD9371 FilterWizard application for a No-OS application. I need to configure the sampling rates for both the Tx and Rx paths.
Could someone provide me with the maximum and minimum sampling rates that can be configured for Tx and Rx using these tools or is there any other tools where I can configure the minimum sampling rate less than 50MHz and above 500MHz?
Specifically:
If there are any additional considerations or constraints when setting these rates, such as specific configurations or limitations based on the sampling rate, I would appreciate that information as well.
Thank you in advance for your help!
__CommunityServer__Service__ - Moved from TES GUI & API Software Support AD9371/AD9375 to Support AD9371/AD9375. Post date updated from Friday, September 13, 2024 1:23 PM UTC to Friday, January 30, 2026 12:13 AM UTC to reflect the move.
What is the maximum and minimum sampling rate that can be set for Tx (transmit) in TES or FilterWizard?
What is the maximum and minimum sampling rate that can be set for Rx (receive) in TES or FilterWizard?
Below are the minimum and maximum sampling rates possible for TX and RX.
https://wiki.analog.com/resources/eval/user-guides/mykonos/software/filters

What is the maximum and minimum sampling rate that can be set for Tx (transmit) in TES or FilterWizard?
What is the maximum and minimum sampling rate that can be set for Rx (receive) in TES or FilterWizard?
Below are the minimum and maximum sampling rates possible for TX and RX.
https://wiki.analog.com/resources/eval/user-guides/mykonos/software/filters

I'm using an external clock source of 30.72 MHz with the AD9371. Will the sampling rate depend on this clock? If I change the clock to 61.44 MHz, will the sampling rate increase accordingly, or are there other factors that determine the sampling rate beyond the external clock frequency?
The sampling rate/IQ rate depends on the input clock and it should be an integer multiple of the input clock.