Post Go back to editing

Maximum and Minimum Sampling Rates for Tx and Rx in AD9371 with TES or FilterWizard application

Thread Summary

The user is configuring sampling rates for the AD9371 RF transceiver using Transceiver Evaluation Software (TES) or FilterWizard. The maximum and minimum sampling rates for both Tx and Rx paths are dependent on the input clock and should be integer multiples of it. For an external clock of 30.72 MHz, the sampling rates are constrained accordingly. Changing the clock to 61.44 MHz will adjust the sampling rates, but specific limits are not provided in the thread.
AI Generated Content
Category: Hardware
Product Number: AD9371

I am currently working with the AD9371 RF transceiver and using either the Transceiver Evaluation Software (TES) or the AD9371 FilterWizard application for a No-OS application. I need to configure the sampling rates for both the Tx and Rx paths.

Could someone provide me with the maximum and minimum sampling rates that can be configured for Tx and Rx using these tools or is there any other tools where I can configure the minimum sampling rate less than 50MHz and above 500MHz?

Specifically:

  1. What is the maximum and minimum sampling rate that can be set for Tx (transmit) in TES or FilterWizard?
  2. What is the maximum and minimum sampling rate that can be set for Rx (receive) in TES or FilterWizard?

If there are any additional considerations or constraints when setting these rates, such as specific configurations or limitations based on the sampling rate, I would appreciate that information as well.

Thank you in advance for your help!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.