| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Missed after 168 hours |
Closed | |
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
I am working on an AD9371 and ZC706 No OS application, configuring the AD9371 transceiver with a fixed device clock of 122.88 MHz. To ensure compatibility with my system, I need to achieve an IQ sample rate that is an integer and less than 49.152 MHz. Is there any TES gui software source, for changing the device clock.
I have attempted to configure the transceiver using the available settings but have not yet achieved the desired integer sample rate below 49.152 MHz. Could anyone confirm if my approach is correct, or if there are any other methods or configurations I should consider to achieve this?
Any insights or suggestions would be greatly appreciated. Thank you!
Dorant - Moved from RF and Microwave to TES GUI & API Software Support AD9371/AD9375. Post date updated from Monday, June 24, 2024 8:36 AM UTC to Friday, July 5, 2024 1:00 PM UTC to reflect the move.
__CommunityServer__Service__ - Moved from TES GUI & API Software Support AD9371/AD9375 to Support AD9371/AD9375. Post date updated from Friday, July 5, 2024 1:00 PM UTC to Friday, January 30, 2026 12:12 AM UTC to reflect the move.
I have been referring to the software filters documentation available on Analog Devices’ wiki (https://wiki.analog.com/resources/eval/user-guides/mykonos/software/filters). According to this documentation, the supported Tx and Rx sampling rates are between 30 MSPS and 320 MSPS.
I need to determine if there is a way to configure the AD9371 for sampling rates outside this range. Specifically:
I have been referring to the software filters documentation available on Analog Devices’ wiki (https://wiki.analog.com/resources/eval/user-guides/mykonos/software/filters). According to this documentation, the supported Tx and Rx sampling rates are between 30 MSPS and 320 MSPS.
I need to determine if there is a way to configure the AD9371 for sampling rates outside this range. Specifically:
Is it possible to set the sampling rate below 30 MSPS or above 320 MSPS for the AD9371?
It is not possible to configure with sampling rates below 30Msps and above 320Msps.
Are there any special configurations, workarounds, or additional software/hardware tools that might allow setting sampling rates outside this specified range?
No
Could you explain the technical reasons behind limiting the AD9371's supported Tx and Rx sampling rates to between 30 MSPS and 320 MSPS? Are these restrictions due to hardware, filter design, or other performance considerations, and is there any potential for extending the supported range through future updates or alternative configurations?
There are no plans as of now to support the rates beyond the specified range.