Post Go back to editing

Configuring AD9371 for Integer IQ Sample Rate Below 49.152 MHz in No OS Application:

Category: Hardware

I am working on an AD9371 and ZC706 No OS application, configuring the AD9371 transceiver with a fixed device clock of 122.88 MHz. To ensure compatibility with my system, I need to achieve an IQ sample rate that is an integer and less than 49.152 MHz.  Is there any TES gui software source, for changing the device clock.

I have attempted to configure the transceiver using the available settings but have not yet achieved the desired integer sample rate below 49.152 MHz. Could anyone confirm if my approach is correct, or if there are any other methods or configurations I should consider to achieve this?

Any insights or suggestions would be greatly appreciated. Thank you!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.