Post Go back to editing

TR MODULE

Category: Software
Product Number: AD9371

Regarding the question of 9371, please consult:

Is it impossible to use the TES of 9371 without an evaluation board? Can you configure parameters, generate related scripts, or initialize structures like 9361?

Can the sampling rate of the transmission and reception interface between 9371 and BBP be flexibly configured, such as the entire 25MSps sampling rate? It's not necessary, it must be something like 30.72/61.44/122.88, right?

What is the final output sampling bit of the RX branch of 9371? 16 bit or 12 bit?

4. The TX branch of 9371, where did I see an input sampling bit of 14 bits written?

5. If the external clock is 20M, can the rx and tx sampling rates achieve 100MSps? How low can it reach?

Thread Notes