Post Go back to editing

B0322J5050AHF for AD9371's TX port

Thread Summary

The user asked if connecting 1.8V to Pin 2 of the Anaren B0322J5050AHF, which is labeled as GND, is an error. The final answer confirmed it is an error and suggested feeding 1.8V through Pin 3 or 4 instead. The accompanying answer provided a schematic and explained that Pin 2 is not used for DC feed in this configuration.
AI Generated Content
Category: Hardware

On page 252 in Fig. 150 it is shown that I can connect Pin 2 of Anaren B0322J5050AHF to the 1.8 V feeding line. However, in Anaren B0322J5050AHF datasheet Pin 2 is stated as GND. Is this an error? and how can i connect 1.8V in a right way to feed the AD9371's TX port . should i connect 1.8V to pin 2, or to pin 3,4?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.