Post Go back to editing

ad9371 ORX noise raised at frequency edges

Thread Summary

The user is experiencing raised noise at the frequency edges of the ORx signal on the AD9371 when using a 245.76 MHz IQ rate and 200 MHz bandwidth. The final answer suggests increasing the oversampling ratio by adjusting the decimation rates of the Half Band and FIR filters to push the noise further and achieve a flatter noise floor. The user also tried bypassing the RFIR and increasing the ORx gain, but the noise shape remained unchanged. The user is advised to use the latest filter wizard to generate profiles and ensure the ORx path is enabled correctly.
AI Generated Content
Category: Hardware
Product Number: ad9371

Settings:

ad9371 orx IQrate 245.76MHz, bandwidth 200MHz, 

Using the following Orx filter config generated by ad9371 filter wizard 

<obs>
<adcDiv=1>
<rxFirDecimation=1>
<rxDec5Decimation=5>
<enHighRejDec5=1>
<rhb1Decimation=1>
<iqRate_kHz=245760>
<rfBandwidth_Hz=200000000>
<rxBbf3dBCorner_kHz=100000>

<filter FIR gain=6 num=24>
-289
81
-23
-86
229
-354
397
-233
-657
1699
-4172
23010
-4172
1699
-657
-233
397
-354
229
-86
-23
81
-289
0
</filter>

But the received orx signal has raised noise at frequency edge.

if i turn off the signal, the noise looks not flat,check the red curve in following figure.

I try some dec5 filter coefs, no big change. 

thanks 

Thread Notes

Parents
  • Hi  ,

    We have also observed same thing in our design. Tx and ORx at 245.76MSPS. Would like to know if your Tx output is clean or are you observing any spurious at offset of 122.88MHz or 245.76MHz from LO. If possible share the spectrum snapshot with 1GHz span. How does the ORX plot look if sine wave is given as input?

    Thanks

Reply
  • Hi  ,

    We have also observed same thing in our design. Tx and ORx at 245.76MSPS. Would like to know if your Tx output is clean or are you observing any spurious at offset of 122.88MHz or 245.76MHz from LO. If possible share the spectrum snapshot with 1GHz span. How does the ORX plot look if sine wave is given as input?

    Thanks

Children