Post Go back to editing

AD9371 power supply

AD9371 Power supply Chains (1.3 V digital, 1.3 V analog, 1.8 V analog, 3.3V analog, VDD_JESD_VTT and VDDA_SER) are derived from ADP5054 where as VDD_IF is derived through an LDO ADP125 from 3.3 V analog supply chain. Is it required to use LDOs for the other supply chains also which are being used directly from ADP5054 now. Please suggest the part if additional LDos are required.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.