Locale Icon
English
EngineerZone
EngineerZone
RF & Microwave
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

RF & Microwave
RF & Microwave
Documents ADL5902 RMS Detector Output Voltage Clamping for High Input Power Levels
  • Q&A
  • File Uploads
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD8363 Recommended for New Designs
The AD8363 is a true rms responding power detector that can be directly driven with a single-ended 50 Ω source. This feature makes the AD8363 frequency...
Datasheet
AD8363 on Analog.com

AD8364 Recommended for New Designs
The AD8364 is a true rms, responding, dual-channel RF power measurement subsystem for the precise measurement and control of signal power. The flexibility...
Datasheet
AD8364 on Analog.com

ADL5902 Recommended for New Designs
The ADL5902 is a true rms responding power detector that has a 65 dB measurement range when driven with a single-ended 50 Ω source. This feature makes...
Datasheet
ADL5902 on Analog.com

AD8362 Production
The AD8362 is a true rms-responding power detector that has a 65 dB measurement range. It is intended for use in a variety of high frequency communication...
Datasheet
AD8362 on Analog.com

Table of Contents
  • +Documents
  • +RF Switches & Attenuators: FAQ
  • +24GHz FMCW Radar: FAQ
  • +AD608: FAQ
  • +AD8302: FAQ
  • +AD8306: FAQ
  • +AD8307: FAQ
  • +AD8309: FAQ
  • +AD8310: FAQ
  • +AD8314: FAQ
  • +AD8318: FAQ
  • +AD8319: FAQ
  • +AD831: FAQ
  • +AD8333: FAQ
  • +AD8339 : FAQ
  • +AD8339: FAQ
  • +AD8340: FAQ
  • +AD8342: FAQ
  • +AD8343: FAQ
  • +AD8345: FAQ
  • +AD8346: FAQ
  • +AD8347: FAQ
  • +AD8348 and ADL5387: FAQ
  • +AD8349: FAQ
  • +AD8361: FAQ
  • +AD8362: FAQ
  • -AD8363: FAQ
    • AD8363: Using INHI vs. INLO for Wideband Applications
    • ADL5902 RMS Detector Output Voltage Clamping for High Input Power Levels
    • Alternatives to  AD8362 High Range RF RMS Detector
    • Can the AD8362 Logarithmic RMS Detector accurately WiMax and LTE?
    • Operating the AD8362 Evaluation Board at Low Frequencies
    • Operating the AD8364 dual RMS Detector at frequencies below 450 MHz
    • Reducing the Response Time of an RMS Detector
    • S-Paramters for a RMS-responding RF Detectors
    • AD8363: Part-to-Part variation
  • +AD8364: FAQ
  • +AD8366: FAQ
  • +AD8368: FAQ
  • +AD8370: FAQ
  • +AD8375: FAQ
  • +AD9854 DDS: FAQ
  • +AD9901: FAQ
  • +ADAR1000: FAQ
  • +ADAR2004: FAQ
  • +ADF4001: FAQ
  • +ADF4002: FAQ
  • +ADF41020: FAQ
  • +ADF4106: FAQ
  • +ADF4107: FAQ
  • +ADF4108: FAQ
  • +ADF4113: FAQ
  • +ADF4118: FAQ
  • +ADF4150: FAQ
  • +ADF4153: FAQ
  • +ADF4155: FAQ
  • +ADF4158: FAQ
  • +ADF4159: FAQ
  • +ADF4193: FAQ
  • +ADF41XX: FAQ
  • +ADF4208: FAQ
  • +ADF4212: FAQ
  • +ADF4252: FAQ
  • +ADF4350 and ADF4351: FAQ
  • +ADF4350: FAQ
  • +ADF4351: FAQ
  • +ADF4355-2: FAQ
  • +ADF4360-0: FAQ
  • +ADF4360-1: FAQ
  • +ADF4360-5: FAQ
  • +ADF4360-6: FAQ
  • +ADF4360-7: FAQ
  • +ADF4360-8: FAQ
  • +ADF4360-9: FAQ
  • +ADF4360-x: FAQ
  • +ADF4371: FAQ
  • +ADF4372: FAQ
  • +ADF4377: FAQ
  • +ADF5355: FAQ
  • +ADF5356: FAQ
  • +ADF5709: FAQ
  • +ADF7021-N: FAQ
  • +ADF9010: FAQ
  • +ADG901: FAQ
  • +ADG904: FAQ
  • +ADG918: FAQ
  • +ADG936: FAQ
  • ADI Products Suitable for Software Defined Radio?
  • +ADIsimRF: FAQ
  • +ADL5240_ADL5243: FAQ
  • +ADL5330: FAQ
  • +ADL5336: FAQ
  • +ADL5350: FAQ
  • +ADL5370: FAQ
  • +ADL5371: FAQ
  • +ADL5373: FAQ
  • +ADL5375-05: FAQ
  • +ADL5375: FAQ
  • +ADL5380: FAQ
  • +ADL5382: FAQ
  • +ADL5385: FAQ
  • +ADL5387: FAQ
  • +ADL5390: FAQ
  • +ADL5502: FAQ
  • +ADL5505: FAQ
  • +ADL5511: FAQ
  • +ADL5513 : FAQ
  • +ADL5513: FAQ
  • +ADL5519: FAQ
  • +ADL5535/6: FAQ
  • +ADL5569 : FAQ
  • +ADL5601/2: FAQ
  • +ADL5602: FAQ
  • +ADL5801 : FAQ
  • +ADL5801: FAQ
  • +ADL5802: FAQ
  • +ADL5902: FAQ
  • +ADL5903: FAQ
  • +ADL5904 : FAQ
  • +ADL5906: FAQ
  • +ADL5920: FAQ
  • +ADL5960 : FAQ
  • +ADL8101: FAQ
  • +ADL8106ACEZ: FAQ
  • +ADL8107 : FAQ
  • +ADL8120: FAQ
  • +ADL8142ACPZN: FAQ
  • +ADMV4530: FAQ
  • +ADMV4630: FAQ
  • +ADMV8526: FAQ
  • +ADPA9002: FAQ
  • +ADPA1107: FAQ
  • +ADPA7009-2: FAQ
  • +ADRF6520: FAQ
  • +ADRF6620: FAQ
  • +ADRF6650 : FAQ
  • +ADRF6703: FAQ
  • +ADRF6755: FAQ
  • +PLL: FAQ
  • +IQ Modulator : FAQ
  • +dc bias level: FAQ
  • +FAQ: ADRF6821
  • +Footprint for ADI components: FAQ
  • +Fractional-N PLLs: FAQ
  • +Gerber files: FAQ
  • +High Voltage VCOs: FAQ
  • +Frequency Dividers: FAQ
  • +Phase Frequency Detectors: FAQ
  • +HMC-ABH241: FAQ
  • +HMC-C019: FAQ
  • +HMC-C030: FAQ
  • +HMC-T2220: FAQ
  • +HMC1013: FAQ
  • +HMC1020: FAQ
  • +HMC1048A: FAQ
  • +HMC1056: FAQ
  • +HMC1110: FAQ
  • +HMC1119 : FAQ
  • +HMC1119: FAQ
  • +HMC156A: FAQ
  • +HMC194: FAQ
  • +HMC241: FAQ
  • +HMC253: FAQ
  • +HMC270AMS8GE: FAQ
  • +HMC273MS10G: FAQ
  • +HMC292A: FAQ
  • +HMC305SLP4E: FAQ
  • +HMC322ALP4E: FAQ
  • +HMC346AMS8GE : FAQ
  • +HMC348: FAQ
  • +HMC399: FAQ
  • +HMC406MS8G: FAQ
  • +HMC414MS8GE?, HMC414: FAQ
  • +HMC440: FAQ
  • +HMC451: FAQ
  • +HMC457 : FAQ
  • +HMC463-Die : FAQ
  • +HMC542BLP4E: FAQ
  • +HMC550: FAQ
  • +HMC554A: FAQ
  • +HMC557A: FAQ
  • +HMC558A: FAQ
  • +HMC574: FAQ
  • +HMC587LC4B: FAQ
  • +HMC589: FAQ
  • +HMC595E: FAQ
  • +HMC611LP4: FAQ
  • +HMC624ALP4E: FAQ
  • +HMC625B: FAQ
  • +HMC634LC4 : FAQ
  • +HMC634LC4: FAQ
  • +HMC641ALP4E: FAQ
  • +HMC685LP4: FAQ
  • +HMC686LP4/686LP4E: FAQ
  • +HMC694LP4 : FAQ
  • +HMC703: FAQ
  • +HMC7044 : FAQ
  • +HMC710: FAQ
  • +HMC739 : FAQ
  • +HMC767: FAQ
  • +HMC769: FAQ
  • +HMC773ALC3B: FAQ
  • +HMC778LP6CE: FAQ
  • +HMC787: FAQ
  • +HMC807LP6CE: FAQ
  • +HMC830: FAQ
  • +HMC832LP6GE vs HMC830LP6GE: FAQ
  • +HMC833: FAQ
  • +HMC8412: FAQ
  • +HMC8415: FAQ
  • +HMC862: FAQ
  • +HMC904LC5: FAQ
  • +HMC905: FAQ
  • +HMC909: FAQ
  • +HMC915LP4ETR: FAQ
  • +HMC917LP3E: FAQ
  • +HMC939: FAQ
  • +HMC986A: FAQ
  • +Int-N PLL evaluation boards: FAQ
  • +IQ Demodulator: FAQ
  • +IQ Modulator: FAQ
  • +LNA: FAQ
  • +LTC5507 : FAQ
  • +LTC5507: FAQ
  • +LTC5510: FAQ
  • +LTC5552 : FAQ
  • +LTC5584, LTC5599: FAQ
  • +LTC694x: FAQ
  • MAX1470: FAQ
  • +MAX1470EUI+_T1: FAQ
  • +MAX1471ATJ/V+: FAQ
  • +MAX1471EVKIT-433: FAQ
  • +MAX1473ETJ+: FAQ
  • +MAX1473EVKIT-315: FAQ
  • +MAX2014: FAQ
  • +MAX2016ETI+: FAQ
  • MAX2112: FAQ
  • +MAX2112CTI+: FAQ
  • +MAX2112EVKIT+: FAQ
  • +MAX2120: FAQ
  • +MAX21210ELD+: FAQ
  • MAX2121B: FAQ
  • +MAX2121BETI+: FAQ
  • +MAX2172ETL/V+TCBM: FAQ
  • +MAX2223 : FAQ
  • +MAX2223ETI+: FAQ
  • +MAX2306EVKIT: FAQ
  • +MAX2606EUT: FAQ
  • MAX2620: FAQ
  • +MAX2620EUA+: FAQ
  • +MAX2623EUA+: FAQ
  • +MAX2680EVKIT#: FAQ
  • +MAX2754: FAQ
  • +MAX2754EUA+: FAQ
  • MAX2769BETI/V+: FAQ
  • +MAX2769BETI/V+_T1: FAQ
  • +MAX2769CC/D+: FAQ
  • +MAX2769CETI+: FAQ
  • +MAX2769CEVKIT#: FAQ
  • +MAX2771 GUI: FAQ
  • MAX2771: FAQ
  • +MAX2771C/D+: FAQ
  • MAX2771ETI+: FAQ
  • +MAX2771ETI+T: FAQ
  • +MAX2771EVKIT#: FAQ
  • +MAX2771_/D+_A1: FAQ
  • +MAX2870 : FAQ
  • +MAX2871 : FAQ
  • +MAX2880 PLL EV KIT SOFTWARE: FAQ
  • +MAX2880ETP+: FAQ
  • +MAX2880EVKIT#: FAQ
  • +MAX4002EBL+: FAQ
  • +MAX4003EUA+: FAQ
  • +MAX41470: FAQ
  • +MAX41473: FAQ
  • MAX7033: FAQ
  • +MAX7033EUI+T: FAQ
  • +MAX7034AUI/V+: FAQ
  • +MAX7036GTP+: FAQ
  • +MAX7036GTP/V+: FAQ
  • +MAX7042ATJ+: FAQ
  • +MAX7042EVKIT: FAQ
  • +OP-AMP: FAQ
  • +RF & Microwave: FAQ
  • +RF Connectors: FAQ
  • +RF Detector Overdrive: FAQ
  • +rms detector: FAQ
  • +S-Parameters: FAQ
  • +SC1894-EVK2400: FAQ
  • +SC1894A-00A00: FAQ
  • +SC1894A-00C13: FAQ
  • +SC2200-EVK1900: FAQ
  • +SC2200-EVK2400: FAQ
  • +AD641: FAQ
  • +AD8309 : FAQ
  • +AD8363 : FAQ
  • +ADA4961 : FAQ
  • +ADAR1000 : FAQ
  • +ADAR2001 : FAQ
  • +ADAR2004 : FAQ
  • +ADAR4002 : FAQ
  • +ADAR4002: FAQ
  • +ADF4150HV : FAQ
  • +ADF41513: FAQ
  • +ADF4158 : FAQ
  • +ADF4159 : FAQ
  • +ADF4368 : FAQ
  • +ADF4368BCCZ, ADF4368: FAQ
  • +ADF4371 : FAQ
  • +ADF4372 : FAQ
  • +ADF4382A : FAQ
  • +ADF4382A: FAQ
  • +ADF4383 : FAQ
  • +ADF5356 : FAQ
  • +ADF5709 : FAQ
  • +ADF5904 : FAQ
  • +ADISimPLL: FAQ
  • +ADL5206 : FAQ
  • +ADL5902 : FAQ
  • +ADL5904-EVALZ, ADL5904: FAQ
  • +ADL8108: FAQ
  • +ADL8112 : FAQ
  • +ADL8201 : FAQ
  • +ADMV1013: FAQ
  • +ADMV1550 : FAQ
  • +ADMV4350: FAQ
  • +ADMV8052 : FAQ
  • +ADMV8052: FAQ
  • +ADMV8818-EVALZ, ADMV8818: FAQ
  • +ADMV8818: FAQ
  • +ADPA7008: FAQ
  • +ADRF5026 : FAQ
  • +ADRF5031 : FAQ
  • +ADRF5040 : FAQ
  • +ADRF5050: FAQ
  • +ADRF5160: FAQ
  • +ADRF5162 : FAQ
  • +ADRF5238 : FAQ
  • +ADRF5730 : FAQ
  • +ADRF5730: FAQ
  • +ADTR1107 : FAQ
  • +ADTR1107: FAQ
  • +EV-ADF4368SD1Z: FAQ
  • +EV-TINYRAD24G: FAQ
  • +EVAL-TINYRAD24G: FAQ
  • +HMC1010: FAQ
  • +HMC1099: FAQ
  • +HMC1118 : FAQ
  • +HMC1163 : FAQ
  • +HMC440 : FAQ
  • +HMC472ALP4E, HMC472A: FAQ
  • +HMC531LP5E, HMC531: FAQ
  • +HMC544A : FAQ
  • +HMC598 : FAQ
  • +HMC698 : FAQ
  • +HMC734 : FAQ
  • +HMC740 : FAQ
  • +HMC784A : FAQ
  • +HMC813-Die : FAQ
  • +HMC849A : FAQ
  • +HMC862A: FAQ
  • +HMC943APM5E: FAQ
  • +HMC980: FAQ
  • +HMC994APM5E : FAQ
  • +HMC994APM5E: FAQ
  • +HMC998APM5E : FAQ
  • +LT5537: FAQ
  • +LT5575 : FAQ
  • +LT5581: FAQ
  • +LTC6433-15 : FAQ
  • +LTC6954 : FAQ
  • +LTP5901-IPM : FAQ
  • +MAX2659 : FAQ
  • +MAX2678 : FAQ
  • +PLL/VCO: FAQ
  • +SC1894 : FAQ
  • +SDP-S: FAQ

ADL5902 RMS Detector Output Voltage Clamping for High Input Power Levels

Q.

At high input power levels (above 0 dBm), the output voltage of the ADL5902 rms detectors (and some other rms detectors also) loses linearity and clamps to the rail. What causes this and is there any way to prevent it?

---------------------------------------------------------------------------------------------------------

A.

The plot below illustrates the effect you are describing. In this case, as the input power approaches +3 dBm,  the output voltage starts increasing rapidly and clamps at a level of around 4.7 V (this clamping  level varies with temperature).

This effect is caused by the internal architecture of the ADL5902.  In its normal operating mode, Vout connects to Vset. This closes an internal AGC loop which uses a VGA to present a constant input level to the internal square law detector (one of the X2 blocks).  As the input level increases, the gain control voltage to the detector (which is also the final output voltage), keeps increasing which causes the gain of the VGA to decrease. When the gain cannot be decreased any further, the AGC loop's integrator voltage (Vout) goes open loop and clamps to the rail (approx 4.7V).

If you do not want the device to behave in this manner, the most practical solution is to increase the slope of the transfer function by connecting a resistor divider between Vout, Vset and ground (as described in the datasheet). This will give higher Vout voltages for a particular input power. So you could set the slope so that the output voltage is equal to 4.6 V for an input level of +3 dBm. If you increase the input level above +3dBm the loop will still open up but the output voltage jump will be much smaller. In this example, the voltage will jump from 4.6 V to approx 4.7V (clamp level varies with temperature).

Tags: ad8362 adl5902 ad8364 ad8363
  • Share
  • History
  • More