Q.
The typical supply current on the ADL5902 is specifed as 73 mA and 90 mA at 25 degC and 125 degC respectively. What is the worst case value?
--------------------------------------------------------------------------------------------------------
A.
The attached plot gives a sense for the part-to-part variation in supply current.
These numbers do not exactly line up with the data sheet typicals for 25 degC or 125 degC. The sample here is a smaller population of devices compared to that used for during full device characterization. As a guideline, if you are planning to use the device up 125 degC, I would suggest budgeting for at least 100 mA for the ADL5902.