Locale Icon
English
EngineerZone
EngineerZone
RF & Microwave
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

RF & Microwave
RF & Microwave
Documents How can I avoid startup transients when operating the AD8318 in Controller Mode?
  • Q&A
  • File Uploads
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD8315 Production
The AD8315 is a complete low cost subsystem for the precise control of RF power amplifiers operating in the frequency range 0.1 GHz to 2.5 GHz and over...
Datasheet
AD8315 on Analog.com

AD8317 Production
The AD8317 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
AD8317 on Analog.com

AD8319 Recommended for New Designs
The AD8319 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
AD8319 on Analog.com

AD8363 Recommended for New Designs
The AD8363 is a true rms responding power detector that can be directly driven with a single-ended 50 Ω source. This feature makes the AD8363 frequency...
Datasheet
AD8363 on Analog.com

AD8314 Production
The AD8314 is a complete low cost subsystem for the measurement and control of RF signals in the frequency range of 100 MHz to 2.7 GHz, with a typical...
Datasheet
AD8314 on Analog.com

AD8364 Recommended for New Designs
The AD8364 is a true rms, responding, dual-channel RF power measurement subsystem for the precise measurement and control of signal power. The flexibility...
Datasheet
AD8364 on Analog.com

AD8311 Recommended for New Designs
The AD8311 is a complete low cost subsystem for the precise control of RF power amplifiers operating in the frequency range 0.1 GHz to 2.5 GHz and over...
Datasheet
AD8311 on Analog.com

AD8318 Recommended for New Designs
The AD8318 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output voltage...
Datasheet
AD8318 on Analog.com

ADL5513S Recommended for New Designs
The ADL5513 is a demodulating logarithmic amplifier, capable of accurately converting an RF input signal to a corresponding decibel-scaled output. It employs...
Datasheet
ADL5513S on Analog.com

AD8312 Recommended for New Designs
The AD8312 is a complete, low cost subsystem for the measurement of RF signals in the frequency range of 50 MHz to 3.5 GHz. It has a typical dynamic range...
Datasheet
AD8312 on Analog.com

ADL5902 Recommended for New Designs
The ADL5902 is a true rms responding power detector that has a 65 dB measurement range when driven with a single-ended 50 Ω source. This feature makes...
Datasheet
ADL5902 on Analog.com

AD8302 Recommended for New Designs
The AD8302 is a fully integrated system for measuring gain/loss and phase in numerous receive, transmit, and instrumentation applications. It requires...
Datasheet
AD8302 on Analog.com

ADL5519 Recommended for New Designs
The ADL5519 is a dual-demodulating logarithmic amplifier that incorporates two AD8317s. It can accurately convert an RF input signal into a corresponding...
Datasheet
ADL5519 on Analog.com

AD8313 Production
The AD8313 is a complete multistage demodulating logarithmic amplifier that can accurately convert an RF signal at its input to an equivalent decibel-scaled...
Datasheet
AD8313 on Analog.com

AD8362 Production
The AD8362 is a true rms-responding power detector that has a 65 dB measurement range. It is intended for use in a variety of high frequency communication...
Datasheet
AD8362 on Analog.com

Table of Contents
  • +Documents
  • +RF Switches & Attenuators: FAQ
  • +24GHz FMCW Radar: FAQ
  • +AD608: FAQ
  • -AD8302: FAQ
    • AD8302 Gain and Phase with no Input Signal
    • AD8302 Gain/Phase Detector, Response to Modulated Signals
    • AD8302 Gain/Phase Detector: Operation as a Frequency Discriminator
    • How can I avoid startup transients when operating the AD8318 in Controller Mode?
    • AD8302 evaluation board information
    • AD8302 Full phase detection
    • AD8302 spice model and gerbers for eval board
    • AD8302's Small Signal Envelope Bandwidth
    • AD8302: Hot to measure +/- 180deg phase
    • AD8302: Offsetting the phase output
    • AD8302: VPHS output changes with different input signal amplitude
    • The permittivity and the thickness of the AD8302’s EVB.
  • +AD8306: FAQ
  • +AD8307: FAQ
  • +AD8309: FAQ
  • +AD8310: FAQ
  • +AD8314: FAQ
  • +AD8318: FAQ
  • +AD8319: FAQ
  • +AD831: FAQ
  • +AD8333: FAQ
  • +AD8339 : FAQ
  • +AD8339: FAQ
  • +AD8340: FAQ
  • +AD8342: FAQ
  • +AD8343: FAQ
  • +AD8345: FAQ
  • +AD8346: FAQ
  • +AD8347: FAQ
  • +AD8348 and ADL5387: FAQ
  • +AD8349: FAQ
  • +AD8361: FAQ
  • +AD8362: FAQ
  • +AD8363: FAQ
  • +AD8364: FAQ
  • +AD8366: FAQ
  • +AD8368: FAQ
  • +AD8370: FAQ
  • +AD8375: FAQ
  • +AD9854 DDS: FAQ
  • +AD9901: FAQ
  • +ADAR1000: FAQ
  • +ADAR2004: FAQ
  • +ADF4001: FAQ
  • +ADF4002: FAQ
  • +ADF41020: FAQ
  • +ADF4106: FAQ
  • +ADF4107: FAQ
  • +ADF4108: FAQ
  • +ADF4113: FAQ
  • +ADF4118: FAQ
  • +ADF4150: FAQ
  • +ADF4153: FAQ
  • +ADF4155: FAQ
  • +ADF4158: FAQ
  • +ADF4159: FAQ
  • +ADF4193: FAQ
  • +ADF41XX: FAQ
  • +ADF4208: FAQ
  • +ADF4212: FAQ
  • +ADF4252: FAQ
  • +ADF4350 and ADF4351: FAQ
  • +ADF4350: FAQ
  • +ADF4351: FAQ
  • +ADF4355-2: FAQ
  • +ADF4360-0: FAQ
  • +ADF4360-1: FAQ
  • +ADF4360-5: FAQ
  • +ADF4360-6: FAQ
  • +ADF4360-7: FAQ
  • +ADF4360-8: FAQ
  • +ADF4360-9: FAQ
  • +ADF4360-x: FAQ
  • +ADF4371: FAQ
  • +ADF4372: FAQ
  • +ADF4377: FAQ
  • +ADF5355: FAQ
  • +ADF5356: FAQ
  • +ADF5709: FAQ
  • +ADF7021-N: FAQ
  • +ADF9010: FAQ
  • +ADG901: FAQ
  • +ADG904: FAQ
  • +ADG918: FAQ
  • +ADG936: FAQ
  • ADI Products Suitable for Software Defined Radio?
  • +ADIsimRF: FAQ
  • +ADL5240_ADL5243: FAQ
  • +ADL5330: FAQ
  • +ADL5336: FAQ
  • +ADL5350: FAQ
  • +ADL5370: FAQ
  • +ADL5371: FAQ
  • +ADL5373: FAQ
  • +ADL5375-05: FAQ
  • +ADL5375: FAQ
  • +ADL5380: FAQ
  • +ADL5382: FAQ
  • +ADL5385: FAQ
  • +ADL5387: FAQ
  • +ADL5390: FAQ
  • +ADL5502: FAQ
  • +ADL5505: FAQ
  • +ADL5511: FAQ
  • +ADL5513 : FAQ
  • +ADL5513: FAQ
  • +ADL5519: FAQ
  • +ADL5535/6: FAQ
  • +ADL5569 : FAQ
  • +ADL5601/2: FAQ
  • +ADL5602: FAQ
  • +ADL5801 : FAQ
  • +ADL5801: FAQ
  • +ADL5802: FAQ
  • +ADL5902: FAQ
  • +ADL5903: FAQ
  • +ADL5904 : FAQ
  • +ADL5906: FAQ
  • +ADL5920: FAQ
  • +ADL5960 : FAQ
  • +ADL8101: FAQ
  • +ADL8106ACEZ: FAQ
  • +ADL8107 : FAQ
  • +ADL8120: FAQ
  • +ADL8142ACPZN: FAQ
  • +ADMV4530: FAQ
  • +ADMV4630: FAQ
  • +ADMV8526: FAQ
  • +ADPA9002: FAQ
  • +ADPA1107: FAQ
  • +ADPA7009-2: FAQ
  • +ADRF6520: FAQ
  • +ADRF6620: FAQ
  • +ADRF6650 : FAQ
  • +ADRF6703: FAQ
  • +ADRF6755: FAQ
  • +PLL: FAQ
  • +IQ Modulator : FAQ
  • +dc bias level: FAQ
  • +FAQ: ADRF6821
  • +Footprint for ADI components: FAQ
  • +Fractional-N PLLs: FAQ
  • +Gerber files: FAQ
  • +High Voltage VCOs: FAQ
  • +Frequency Dividers: FAQ
  • +Phase Frequency Detectors: FAQ
  • +HMC-ABH241: FAQ
  • +HMC-C019: FAQ
  • +HMC-C030: FAQ
  • +HMC-T2220: FAQ
  • +HMC1013: FAQ
  • +HMC1020: FAQ
  • +HMC1048A: FAQ
  • +HMC1056: FAQ
  • +HMC1110: FAQ
  • +HMC1119 : FAQ
  • +HMC1119: FAQ
  • +HMC156A: FAQ
  • +HMC194: FAQ
  • +HMC241: FAQ
  • +HMC253: FAQ
  • +HMC270AMS8GE: FAQ
  • +HMC273MS10G: FAQ
  • +HMC292A: FAQ
  • +HMC305SLP4E: FAQ
  • +HMC322ALP4E: FAQ
  • +HMC346AMS8GE : FAQ
  • +HMC348: FAQ
  • +HMC399: FAQ
  • +HMC406MS8G: FAQ
  • +HMC414MS8GE?, HMC414: FAQ
  • +HMC440: FAQ
  • +HMC451: FAQ
  • +HMC457 : FAQ
  • +HMC463-Die : FAQ
  • +HMC542BLP4E: FAQ
  • +HMC550: FAQ
  • +HMC554A: FAQ
  • +HMC557A: FAQ
  • +HMC558A: FAQ
  • +HMC574: FAQ
  • +HMC587LC4B: FAQ
  • +HMC589: FAQ
  • +HMC595E: FAQ
  • +HMC611LP4: FAQ
  • +HMC624ALP4E: FAQ
  • +HMC625B: FAQ
  • +HMC634LC4 : FAQ
  • +HMC634LC4: FAQ
  • +HMC641ALP4E: FAQ
  • +HMC685LP4: FAQ
  • +HMC686LP4/686LP4E: FAQ
  • +HMC694LP4 : FAQ
  • +HMC703: FAQ
  • +HMC7044 : FAQ
  • +HMC710: FAQ
  • +HMC739 : FAQ
  • +HMC767: FAQ
  • +HMC769: FAQ
  • +HMC773ALC3B: FAQ
  • +HMC778LP6CE: FAQ
  • +HMC787: FAQ
  • +HMC807LP6CE: FAQ
  • +HMC830: FAQ
  • +HMC832LP6GE vs HMC830LP6GE: FAQ
  • +HMC833: FAQ
  • +HMC8412: FAQ
  • +HMC8415: FAQ
  • +HMC862: FAQ
  • +HMC904LC5: FAQ
  • +HMC905: FAQ
  • +HMC909: FAQ
  • +HMC915LP4ETR: FAQ
  • +HMC917LP3E: FAQ
  • +HMC939: FAQ
  • +HMC986A: FAQ
  • +Int-N PLL evaluation boards: FAQ
  • +IQ Demodulator: FAQ
  • +IQ Modulator: FAQ
  • +LNA: FAQ
  • +LTC5507 : FAQ
  • +LTC5507: FAQ
  • +LTC5510: FAQ
  • +LTC5552 : FAQ
  • +LTC5584, LTC5599: FAQ
  • +LTC694x: FAQ
  • MAX1470: FAQ
  • +MAX1470EUI+_T1: FAQ
  • +MAX1471ATJ/V+: FAQ
  • +MAX1471EVKIT-433: FAQ
  • +MAX1473ETJ+: FAQ
  • +MAX1473EVKIT-315: FAQ
  • +MAX2014: FAQ
  • +MAX2016ETI+: FAQ
  • MAX2112: FAQ
  • +MAX2112CTI+: FAQ
  • +MAX2112EVKIT+: FAQ
  • +MAX2120: FAQ
  • +MAX21210ELD+: FAQ
  • MAX2121B: FAQ
  • +MAX2121BETI+: FAQ
  • +MAX2172ETL/V+TCBM: FAQ
  • +MAX2223 : FAQ
  • +MAX2223ETI+: FAQ
  • +MAX2306EVKIT: FAQ
  • +MAX2606EUT: FAQ
  • MAX2620: FAQ
  • +MAX2620EUA+: FAQ
  • +MAX2623EUA+: FAQ
  • +MAX2680EVKIT#: FAQ
  • +MAX2754: FAQ
  • +MAX2754EUA+: FAQ
  • MAX2769BETI/V+: FAQ
  • +MAX2769BETI/V+_T1: FAQ
  • +MAX2769CC/D+: FAQ
  • +MAX2769CETI+: FAQ
  • +MAX2769CEVKIT#: FAQ
  • +MAX2771 GUI: FAQ
  • MAX2771: FAQ
  • +MAX2771C/D+: FAQ
  • MAX2771ETI+: FAQ
  • +MAX2771ETI+T: FAQ
  • +MAX2771EVKIT#: FAQ
  • +MAX2771_/D+_A1: FAQ
  • +MAX2870 : FAQ
  • +MAX2871 : FAQ
  • +MAX2880 PLL EV KIT SOFTWARE: FAQ
  • +MAX2880ETP+: FAQ
  • +MAX2880EVKIT#: FAQ
  • +MAX4002EBL+: FAQ
  • +MAX4003EUA+: FAQ
  • +MAX41470: FAQ
  • +MAX41473: FAQ
  • MAX7033: FAQ
  • +MAX7033EUI+T: FAQ
  • +MAX7034AUI/V+: FAQ
  • +MAX7036GTP+: FAQ
  • +MAX7036GTP/V+: FAQ
  • +MAX7042ATJ+: FAQ
  • +MAX7042EVKIT: FAQ
  • +OP-AMP: FAQ
  • +RF & Microwave: FAQ
  • +RF Connectors: FAQ
  • +RF Detector Overdrive: FAQ
  • +rms detector: FAQ
  • +S-Parameters: FAQ
  • +SC1894-EVK2400: FAQ
  • +SC1894A-00A00: FAQ
  • +SC1894A-00C13: FAQ
  • +SC2200-EVK1900: FAQ
  • +SC2200-EVK2400: FAQ
  • +AD641: FAQ
  • +AD8309 : FAQ
  • +AD8363 : FAQ
  • +ADA4961 : FAQ
  • +ADAR1000 : FAQ
  • +ADAR2001 : FAQ
  • +ADAR2004 : FAQ
  • +ADAR4002 : FAQ
  • +ADAR4002: FAQ
  • +ADF4150HV : FAQ
  • +ADF41513: FAQ
  • +ADF4158 : FAQ
  • +ADF4159 : FAQ
  • +ADF4368 : FAQ
  • +ADF4368BCCZ, ADF4368: FAQ
  • +ADF4371 : FAQ
  • +ADF4372 : FAQ
  • +ADF4382A : FAQ
  • +ADF4382A: FAQ
  • +ADF4383 : FAQ
  • +ADF5356 : FAQ
  • +ADF5709 : FAQ
  • +ADF5904 : FAQ
  • +ADISimPLL: FAQ
  • +ADL5206 : FAQ
  • +ADL5902 : FAQ
  • +ADL5904-EVALZ, ADL5904: FAQ
  • +ADL8108: FAQ
  • +ADL8112 : FAQ
  • +ADL8201 : FAQ
  • +ADMV1013: FAQ
  • +ADMV1550 : FAQ
  • +ADMV4350: FAQ
  • +ADMV8052 : FAQ
  • +ADMV8052: FAQ
  • +ADMV8818-EVALZ, ADMV8818: FAQ
  • +ADMV8818: FAQ
  • +ADPA7008: FAQ
  • +ADRF5026 : FAQ
  • +ADRF5031 : FAQ
  • +ADRF5040 : FAQ
  • +ADRF5050: FAQ
  • +ADRF5160: FAQ
  • +ADRF5162 : FAQ
  • +ADRF5238 : FAQ
  • +ADRF5730 : FAQ
  • +ADRF5730: FAQ
  • +ADTR1107 : FAQ
  • +ADTR1107: FAQ
  • +EV-ADF4368SD1Z: FAQ
  • +EV-TINYRAD24G: FAQ
  • +EVAL-TINYRAD24G: FAQ
  • +HMC1010: FAQ
  • +HMC1099: FAQ
  • +HMC1118 : FAQ
  • +HMC1163 : FAQ
  • +HMC440 : FAQ
  • +HMC472ALP4E, HMC472A: FAQ
  • +HMC531LP5E, HMC531: FAQ
  • +HMC544A : FAQ
  • +HMC598 : FAQ
  • +HMC698 : FAQ
  • +HMC734 : FAQ
  • +HMC740 : FAQ
  • +HMC784A : FAQ
  • +HMC813-Die : FAQ
  • +HMC849A : FAQ
  • +HMC862A: FAQ
  • +HMC943APM5E: FAQ
  • +HMC980: FAQ
  • +HMC994APM5E : FAQ
  • +HMC994APM5E: FAQ
  • +HMC998APM5E : FAQ
  • +LT5537: FAQ
  • +LT5575 : FAQ
  • +LT5581: FAQ
  • +LTC6433-15 : FAQ
  • +LTC6954 : FAQ
  • +LTP5901-IPM : FAQ
  • +MAX2659 : FAQ
  • +MAX2678 : FAQ
  • +PLL/VCO: FAQ
  • +SC1894 : FAQ
  • +SDP-S: FAQ

How can I avoid startup transients when operating the AD8318 in Controller Mode?

Q.

How can I avoid startup transients when operating the AD8318 in Controller Mode?  I am using the AD8318 Log Detector/Controller to control  the output level in an AGC loop.  The control loop consists of a fixed-gain  RF amplifier, an ADL5330 VGA, and  the  AD8318 Log Amp.  The circuit is similar to Figure 37 on Page 16 of the ADL5330 data sheet, except with the fixed gain amplifier inserted after the ADL5330 VGA.  I am seeing a startup transient at the output of the RF amplifier.  During startup, the detector is seeing no signal at the amplifier output. This causes the VGA go max gain, producing the transient at the RF amplifier output  that is present until the loop settles.  Is it ok to short the CLPF pin to ground during startup to prevent this transient?

--------------------------------------------------------------------------------------------------------------

A.

The CLPF node is internally fed by a current mirror. By connecting the CLPF node directly to ground, overtime  a transistor in this circuit will degrade and eventually fail. The problem is the Vbceo of the transistor is exceeded.

A better solution to minimize the transient  during the power up sequence is to force the VGA to minimum gain.  During initialization, enable / disable the circuit using the enable pin on the ADL5330. Before enabling the VGA bring the VSET voltage on the AD8318 to 2.5 V. This translates to a power level well below the minimum detectable power of the AD8318. As a result the gain of the ADL5330 will be set to its minimum eliminating the severe overshoot.

Tags: ad8318 ad8319 ad8312 ad8311 ad8317 ad8314 rf_level_control ad8362 adl5513 adl5902 ad8364 ad8315 and ad8363 ad8316 ad8302 ad8313 adl5519 Show More
  • Share
  • History
  • More