Locale Icon
English
EngineerZone
EngineerZone
RF & Microwave
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

RF & Microwave
RF & Microwave
Documents Digital Lock Detect output from the ADF4106 is not indicating lock correctly, why?
  • Q&A
  • File Uploads
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

ADF4107 Production
The ADF4107 frequency synthesizer can be used to implement local oscillators in the up-conversion and down-conversion sections of wireless receivers and...
Datasheet
ADF4107 on Analog.com

ADF41020 Not Recommended for New Designs
The ADF41020 frequency synthesizer can be used to implement local oscillators as high as 18 GHz in the up conversion and down conversion sections of wireless...
ADF41020 on Analog.com

ADF4106 Production
The ADF4106 frequency synthesizer can be used to implement local oscillators in the up-conversion and down-conversion sections of wireless receivers and...
Datasheet
ADF4106 on Analog.com

Table of Contents
  • +Documents
  • +RF Switches & Attenuators: FAQ
  • +1/f noise of the ADL5387: FAQ
  • +1/f phase noise: FAQ
  • +24GHz FMCW Radar: FAQ
  • +AD608: FAQ
  • +AD8302: FAQ
  • +AD8306: FAQ
  • +AD8307: FAQ
  • +AD8309: FAQ
  • +AD8310: FAQ
  • +AD8314: FAQ
  • +AD8318: FAQ
  • +AD8319: FAQ
  • +AD831: FAQ
  • +AD8333: FAQ
  • +AD8339 : FAQ
  • +AD8339: FAQ
  • +AD8340: FAQ
  • +AD8342: FAQ
  • +AD8343: FAQ
  • +AD8345: FAQ
  • +AD8346: FAQ
  • +AD8347: FAQ
  • +AD8348 and ADL5387: FAQ
  • +AD8349: FAQ
  • +AD8361: FAQ
  • +AD8362: FAQ
  • +AD8363: FAQ
  • +AD8364: FAQ
  • +AD8366: FAQ
  • +AD8368: FAQ
  • +AD8370: FAQ
  • +AD8375: FAQ
  • +AD9854 DDS: FAQ
  • +AD9901: FAQ
  • +ADAR1000: FAQ
  • +ADAR2004: FAQ
  • +ADF4001: FAQ
  • +ADF4002: FAQ
  • +ADF41020: FAQ
  • +ADF4106: FAQ
  • -ADF4107: FAQ
    • ADF4107: Phase noise
    • Changing the ADF410X output channel without a glitch?
    • Digital Lock Detect output from the ADF4106 is not indicating lock correctly, why?
    • Explain how the ADF41XX datasheet PLL noise is specified?
    • Q: What happens to the PLL when the REFIN is removed ?.
  • +ADF4108: FAQ
  • +ADF4113: FAQ
  • +ADF4118: FAQ
  • +ADF4150: FAQ
  • +ADF4153: FAQ
  • +ADF4155: FAQ
  • +ADF4158: FAQ
  • +ADF4159: FAQ
  • +ADF4193: FAQ
  • +ADF41XX: FAQ
  • +ADF4208: FAQ
  • +ADF4212: FAQ
  • +ADF4252: FAQ
  • +ADF4350 and ADF4351: FAQ
  • +ADF4350: FAQ
  • +ADF4351: FAQ
  • +ADF4355-2: FAQ
  • ADF435x New boards
  • +ADF4360-0: FAQ
  • +ADF4360-1: FAQ
  • +ADF4360-5: FAQ
  • +ADF4360-6: FAQ
  • +ADF4360-7: FAQ
  • +ADF4360-8: FAQ
  • +ADF4360-9: FAQ
  • +ADF4360-x: FAQ
  • +ADF4372: FAQ
  • +ADF4377: FAQ
  • +ADF5355: FAQ
  • +ADF5356: FAQ
  • +ADF5709: FAQ
  • +ADF7021-N: FAQ
  • +ADF9010: FAQ
  • +ADG901: FAQ
  • +ADG904: FAQ
  • +ADG918: FAQ
  • +ADG936: FAQ
  • ADI Products Suitable for Software Defined Radio?
  • +ADI's RF/IF gain blocks: FAQ
  • +ADIsimRF: FAQ
  • +ADL5240_ADL5243: FAQ
  • +ADL5330: FAQ
  • +ADL5336: FAQ
  • +ADL5350: FAQ
  • +ADL5370: FAQ
  • +ADL5371: FAQ
  • +ADL5373: FAQ
  • +ADL5375-05: FAQ
  • +ADL5375: FAQ
  • +ADL5380: FAQ
  • +ADL5382: FAQ
  • +ADL5385: FAQ
  • +ADL5387: FAQ
  • +ADL5390: FAQ
  • +ADL5502: FAQ
  • +ADL5505: FAQ
  • +ADL5511: FAQ
  • +ADL5513 : FAQ
  • +ADL5513: FAQ
  • +ADL5519: FAQ
  • +ADL5535/6: FAQ
  • +ADL5569 : FAQ
  • +ADL5601/2: FAQ
  • +ADL5602: FAQ
  • +ADL5801 : FAQ
  • +ADL5801: FAQ
  • +ADL5802: FAQ
  • +ADL5902: FAQ
  • +ADL5903: FAQ
  • +ADL5904 : FAQ
  • +ADL5906: FAQ
  • +ADL5920: FAQ
  • +ADL5960 : FAQ
  • +ADL8101: FAQ
  • +ADL8106ACEZ: FAQ
  • +ADL8107 : FAQ
  • +ADL8120: FAQ
  • +ADMV4530: FAQ
  • +ADMV8526: FAQ
  • +ADPA1107: FAQ
  • +ADPA7009-2: FAQ
  • +ADRF6520: FAQ
  • +ADRF6620: FAQ
  • +ADRF6650 : FAQ
  • +ADRF6703: FAQ
  • +ADRF6755: FAQ
  • +Auxiliary DACs: FAQ
  • +Calculating VSWR: FAQ
  • Can the ADMV4530 development kit be used to process L band signals (1-2 GHz), and if not, what is a suitable alternative?
  • +CyUSB PLL: FAQ
  • +DAC/IQ Modulator Combination: FAQ
  • +dc bias level: FAQ
  • +Decoupling(Bypass) and AC-Coupling Capacitors: FAQ
  • EV-TINYRAD24G Linux Drivers
  • +FAQ: ADRF6821
  • FAQ: in a PLL active loop filter, what effect does the op amp bias current have?
  • +Footprint for ADI components: FAQ
  • +Fractional-N PLLs: FAQ
  • +Gerber files: FAQ
  • +High Voltage VCOs: FAQ
  • +HMC Microwave Frequency Dividers: FAQ
  • +HMC Phase Frequency Detectors: FAQ
  • HMC PLL Design Tool V1.15
  • +HMC PLL's & PLLVCO: FAQ
  • +HMC-ABH241: FAQ
  • +HMC-C019: FAQ
  • +HMC-C030: FAQ
  • +HMC-T2220: FAQ
  • +HMC1013: FAQ
  • +HMC1020: FAQ
  • +HMC1048A: FAQ
  • +HMC1056: FAQ
  • +HMC1110: FAQ
  • +HMC1119 : FAQ
  • +HMC1119: FAQ
  • +HMC156A: FAQ
  • +HMC194: FAQ
  • +HMC241: FAQ
  • +HMC253: FAQ
  • +HMC270AMS8GE: FAQ
  • +HMC273MS10G: FAQ
  • +HMC292A: FAQ
  • +HMC305SLP4E: FAQ
  • +HMC322ALP4E: FAQ
  • +HMC346AMS8GE : FAQ
  • +HMC348: FAQ
  • +HMC399: FAQ
  • +HMC406MS8G: FAQ
  • +HMC414MS8GE?, HMC414: FAQ
  • +HMC440: FAQ
  • +HMC451: FAQ
  • +HMC457 : FAQ
  • +HMC463-Die : FAQ
  • +HMC542BLP4E: FAQ
  • +HMC550: FAQ
  • +HMC554A: FAQ
  • +HMC557A: FAQ
  • +HMC558A: FAQ
  • +HMC574: FAQ
  • +HMC587LC4B: FAQ
  • +HMC589: FAQ
  • +HMC595E: FAQ
  • +HMC611LP4: FAQ
  • +HMC624ALP4E: FAQ
  • +HMC625B: FAQ
  • +HMC634LC4 : FAQ
  • +HMC634LC4: FAQ
  • +HMC641ALP4E: FAQ
  • +HMC685LP4: FAQ
  • +HMC686LP4/686LP4E: FAQ
  • +HMC694LP4 : FAQ
  • +HMC703: FAQ
  • +HMC7044 : FAQ
  • +HMC710: FAQ
  • +HMC739 : FAQ
  • +HMC767: FAQ
  • +HMC769: FAQ
  • +HMC773ALC3B: FAQ
  • +HMC778LP6CE: FAQ
  • +HMC787: FAQ
  • +HMC807LP6CE: FAQ
  • +HMC830: FAQ
  • +HMC832LP6GE vs HMC830LP6GE: FAQ
  • +HMC833: FAQ
  • +HMC8412: FAQ
  • +HMC8415: FAQ
  • +HMC862: FAQ
  • +HMC904LC5: FAQ
  • +HMC905: FAQ
  • +HMC909: FAQ
  • +HMC915LP4ETR: FAQ
  • +HMC917LP3E: FAQ
  • +HMC939: FAQ
  • +HMC986A: FAQ
  • How can I suppress in-band spurs such as 3*LO, 4*LO, and 5*LO when using the ADMV1013?
  • How can I use my existing Custom Devices with the latest ADISimRF release, given that the Noise Gain parameter is not coherent with the Gain value and the database is encrypted?
  • How does placing a 1 kO resistor on the control line of ADRF5730 affect the switching time, and what are the implications for the power-up sequencing?
  • +Int-N PLL evaluation boards: FAQ
  • +IQ demodulator: FAQ
  • +IQ Modulators: FAQ
  • Is it safe to set VGG1 to -0.65V before turning on VDD for the ADPA7008, and what are the benefits and downsides of using an active bias controller like HMC980?
  • +LNA: FAQ
  • +LTC5507 : FAQ
  • +LTC5507: FAQ
  • +LTC5510: FAQ
  • +LTC5552 : FAQ
  • LTC5584 : FAQ
  • +LTC5584, LTC5599: FAQ
  • +LTC694x: FAQ
  • Matching Components for HMC1010
  • MAX1470: FAQ
  • +MAX1470EUI+_T1: FAQ
  • +MAX1471ATJ/V+: FAQ
  • +MAX1471EVKIT-433: FAQ
  • +MAX1473ETJ+: FAQ
  • +MAX1473EVKIT-315: FAQ
  • +MAX2014: FAQ
  • +MAX2016ETI+: FAQ
  • MAX2112: FAQ
  • +MAX2112CTI+: FAQ
  • +MAX2112EVKIT+: FAQ
  • +MAX2120: FAQ
  • +MAX21210ELD+: FAQ
  • MAX2121B: FAQ
  • +MAX2121BETI+: FAQ
  • +MAX2172ETL/V+TCBM: FAQ
  • +MAX2223 : FAQ
  • +MAX2223ETI+: FAQ
  • +MAX2306EVKIT: FAQ
  • +MAX2606EUT: FAQ
  • MAX2620: FAQ
  • +MAX2620EUA+: FAQ
  • +MAX2623EUA+: FAQ
  • +MAX2680EVKIT#: FAQ
  • +MAX2754: FAQ
  • +MAX2754EUA+: FAQ
  • MAX2769BETI/V+: FAQ
  • +MAX2769BETI/V+_T1: FAQ
  • +MAX2769CC/D+: FAQ
  • +MAX2769CETI+: FAQ
  • +MAX2769CEVKIT#: FAQ
  • +MAX2771 GUI: FAQ
  • MAX2771: FAQ
  • +MAX2771C/D+: FAQ
  • MAX2771ETI+: FAQ
  • +MAX2771ETI+T: FAQ
  • +MAX2771EVKIT#: FAQ
  • +MAX2771_/D+_A1: FAQ
  • MAX2870: FAQ
  • +MAX2870ETJ+: FAQ
  • MAX2871: FAQ
  • +MAX2871ETJ+: FAQ
  • +MAX2880 PLL EV KIT SOFTWARE: FAQ
  • +MAX2880ETP+: FAQ
  • +MAX2880EVKIT#: FAQ
  • +MAX4002EBL+: FAQ
  • +MAX4003EUA+: FAQ
  • +MAX41470: FAQ
  • +MAX41473: FAQ
  • MAX7033: FAQ
  • +MAX7033EUI+T: FAQ
  • +MAX7034AUI/V+: FAQ
  • +MAX7036GTP+: FAQ
  • +MAX7036GTP/V+: FAQ
  • +MAX7042ATJ+: FAQ
  • +MAX7042EVKIT: FAQ
  • +OP-AMP: FAQ
  • +PLL USB adapter board: FAQ
  • Recommended regulators for ADI PLLs and VCOs
  • +RF & Microwave: FAQ
  • +RF Connectors: FAQ
  • +RF Detector Overdrive: FAQ
  • +rms detector: FAQ
  • +S-Parameters: FAQ
  • +SC1894-EVK2400: FAQ
  • +SC1894A-00A00: FAQ
  • +SC1894A-00C13: FAQ
  • +SC2200-EVK1900: FAQ
  • +SC2200-EVK2400: FAQ
  • SC2200: FAQ
  • +Standard S-Parameter Files: FAQ
  • Why are the NF, Output NSD, Noise Floor, and SNR displayed as infinity in ADIsimRF when opening the ADMFM2000.sgc example file, and how can this be resolved?
  • Why is ADISimRF Rev2.0.0.19 unstable and giving errors when adding devices to the signal chain?

Digital Lock Detect output from the ADF4106 is not indicating lock correctly, why?

The ADF41XX family of integer –N PLL synthesizers offer two forms of lock detect: Analog Lock Detect ( ALD) and Digital Lock Detect ( DLD). The AN-873 application note explains both options to allow the user to make an informed decision as to which form of lock detect to use.

The Phase Frequency Detector (PFD) produces outputs UP and DN in response to the frequency and phase difference at the inputs, namely the R counter and N counter outputs. The logical NOR of UP and DN is used as the source signal for both the ALD and DLD circuits.

 

Figure 1. PFD and Charge Pump on the ADF4xxx Family of PLL Synthesizers

The logical NOR of the PFD outputs in a locked state produces a logic high with low pulses, whose duration is set by the anti-backlash pulse width plus any additional leakage currents.

 

Figure 2. Timing Diagram of PLL in Lock Showing the Reference Signal, Divided RF Signal, Q1 and Q2 (the Up and Down Pulses Going from the PFD to the Charge Pump), and the ALD Signal, which is the NOR of Q1 and Q2

Leakage currents can have a number of sources, most prominent are, VCXO’s, the charge pump, loop filter capacitors, and biasing currents for active loop filters.

After filtering, ALD can have more than just a 0 or 1 representation of a PLL lock status. The output voltage level can more accurately portray the lock status, however, the filter must be designed carefully, and the rise and fall times of the output voltage level can be an issue in some applications. ADIsimPLL can be used to design the ALD external filter components.

Digital lock detect is a CMOS logic output, whose status is logic high for a PLL lock.  By its digital nature, DLD has to make a definite yes-or-no decision as to whether or not a PLL is in lock. Under certain circumstances, as described in application note AN-873, DLD is susceptible to inaccuracies. Through careful consideration of the PFD frequency and leakage currents flowing, it is possible to determine if DLD is accurate in a particular application.

The Digital lock Detect circuit uses the logical NOR of the PFD outputs as its CLKIN source.

 

 

Figure 3. Simplified Circuit Diagram for Digital Lock Detect; CLKIN is the Analog Lock Detect Signal

 

As mentioned, this signal will have low going pulses, whose width will change depending on the anti-backlash pulse and leakage currents. In fact, the leakage currents act to increase the pulse width from its nominal value (which is the anti-backlash pulse width).

The Digital lock detect circuit uses a set window of 15nsec pulse width to determine the lock status of the PLL. When CLKIN of the DLD circuit has a pulse width of less than 15nsec for 5 consecutive cycles, the DLD circuit indicates that the PLL is locked.

Once the DLD circuit indicates lock, it now looks for a loss of lock. The loss of lock is detected when the pulse width of the CLKIN to the DLD circuit is equal to or greater than 30nsec on any subsequent PFD cycle.

In applications where the leakage currents are large enough to increase the pulse width duration of CLKIN to greater than 15nsec, then DLD will not be able to indicate lock, even if the PLL is locked. In this case, the use of ALD is necessary.

The set window for digital lock detect and loss of lock does not change over the usable PFD frequency change. Therefore it’s obvious that the accuracy of the digital lock detect is a function of the PFD frequency. The higher PFD frequency, the shorter will be the periods of the R counter and N counter signal to the PFD.

Taking an example of a PFD frequency = 30MHz, the R and N counter periods will be equal to approximately 33nsec. In this case the accuracy of the digital lock is compromised as the unlocked frequency close to the desired frequency will cause the CLKIN feeding the DLD circuit to drift in and out of the 15nsec window. In this scenario the DLD signal will pulse high and low. In a more extreme case, using a PFD=100MHz, will result in signals at the PFD with a period of 10nsec. A frequency error in this application of 10 % would put the two PFD inputs within 1nsec of each other and the DLD will inaccurately indicate lock detect. In this application it is necessary to use ALD instead of DLD to indicate lock.

Tags: digital lock detect adf4107 adf4102 adf4106 adf4101